NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I use stm32wb5x_BLE_Stack_full_fw.bin v1.13.2 on STM32WB5MMG.The installation address is 0x080CF000.What happens if I write the stack to the wrong address (0x080C7000, the install address for v 1.13.0).In my board, it looks work fine. Is there any co...
Hello, I'm STM F/W Beginner .Recently, I was tasked with a project to implement BLE with the Stm32wb MCU.As a result of referring to Example such as Heartrates or P2PServer Projects, I could successfully send Data to a mobile phone by Nucleo Board.Ho...
Hello all, I made custom PCB board with STM32WB5MMG in my project. I have confirmed that the SWD pins are working and Code is Debugging ok.I have also set up HSEM, IPCC, RCC, RTC, RF, STM32_WPAN required but I can't detect the Blue...
Good morning,I am using an STM32 WL55JC1 starting from the end node example.I am unable to figure out in the code how to set how long or how many tries it makes before it stops trying to connect to the gateawy.Could you please point me to this inform...
i set fido related services and characteristics using cube mx for stm32wb55 development board why i am not getting any value in my coustum event handler.
Hi ,I'm trying to Perform OTA update using ST BLE ToolBox ,I have programmed my STM32WB5MMG with the OTA binary.The problem comes when starting the update process. With ST BLE Sensor there is no problem: the device is updated to the new version of th...
@ST Community @STTwo-32 @Tinnagit @Tesla DeLorean 1) I have done few changes from "#define LORAWAN_DEFAULT_CLASS CLASS_A" to "#define LORAWAN_DEFAULT_CLASS CLASS_C" in the "lora_app.h" file and I also changed "#define DISABLE_LORAWAN_RX_WINDOW 0" to ...
Hello.I have encountered an issue during the migration from STM32WB5MMG to STM32WB1MMC.When I generate the default code using CubeMX with STM32WB1MMC, no errors occur. However, when I try to transfer the code I was using with STM32WB5MMG to STM32WB1M...
Do I need to set the net impedances of differential pair from RFI_P and RFI_N to 50ohm?
Hi.I'm using stm32wb55 MCU.ADC is running in continuous mode with 6 channels using DMA for the results. I want to use analog watchdog interrupt on just 1 channel that is on rank 2.I have 2 problems, first the interrupts occured only for the channel i...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.