NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi, I'm using the APP_LOG function to print data to serial. Here's how i do it:APP_LOG(TS_OFF, VLEVEL_L, "%d,%d,%d,%d,%d,", front_brake_pressure, rear_left_wheel_speed, rear_right_wheel_speed, front_left_wheel_speed, front_right_wheel_speed);APP_LOG(...
HiI use free-rtos with stm32wb55.I use some queues, they all behave as expected except for one of them (led driver queue).It seemed that some of the messages being sent (to the led driver queue) are ignored or missed.I added a debug code and found ou...
Hello everyone,I'm looking to built my own lorawan network. Currently I'm using loriot server. As we need to pay these server. I'm looking to build my own.Looking for the help/guidance on do we need any type of access or permission from these gateway...
Hello everyoneI'm trying to using/operate L072Z LRWAN1 in class c. I'm able to know that node is operating in class c( I'm attaching images below). But i want to disable the receiving window to get faster data rate. In class A I'm getting 20 frames p...
I am using Zigbee for wireless communication using Zigbee_OnOff_Router_NVM as a reference. The problem I am currently facing is that if I turn off the Router for a long time, it may take about 20 seconds for the data to reach the Coordinator the next...
Hi ST Support Team,I am reaching out regarding an issue I have encountered while attempting to utilize USB CCID functionality on the STM32WB55 MCU. Recently, I integrated the CCID driver from the following link into my project.https://github.com/STMi...
Hello, I am developing a device using STM32WL chipset.I'm currently taking the FCC certification test, but it failed in R.S.E (Radio spurious emmision), so I've been reviewing it for 3 weeks.There was an FCC certification logo on the STM32WL Ev-kit, ...
Appreciate pointer to simpliest example for STM32CubeWL sequencer.Specially "Task registration and execution" and "Wait for an event and set event" to do the below sequence. I have AN5406 and reading.....read temperature sensor, transmit on STM32WL...
Which ST Link programmer is best for STM32WL5JC (Lora MCU) for advanced debug facility (still reading, ??trace, monitor??)TIA
How to setup debug session with C breakpoint, stepping, variable read/write, etc. (and advanced facility like monitor, etc. I am still reading...)TIA
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.