2024-04-01 12:41 PM
Which ST Link programmer is best for STM32WL5JC (Lora MCU) for advanced debug facility (still reading, ??trace, monitor??)
TIA
Solved! Go to Solution.
2024-04-02 8:50 AM
PB3 = JTDO / TRACE SWO
2024-04-02 1:23 AM
Hello @David_
I will recommend you to use the STLINK-V3SET. But you still can use other STLINKs (just make sure you are using an original one and not a clone (specially for the STLINK-V2)).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-02 6:31 AM
Many thanks. I read UM2448 Rev 8, page 24/51. Is it correct that I should connect
SWDIO (of STLINK_V3SET) to PA13 (of STM32WL5JC),
SWCLK (of STLINK_V3SET) to PA14 (of STM32WL5JC),
NRST (of STLINK_V3SET) to NRST (of STM32WL5JC),
GND (of STLINK_V3SET) to GND (of STM32WL5JC)
Pin 1 of STLINK_V3SET is stated as INPUT. Is that used by STLINK_V3SET to sense the supply voltage of the target board? I should connect Pin 1 of STLINK_V3SET to the 3.3 volts supply line of the target board, right?
The STM32WL5JC does NOT has a pin named SWO. Hence, Serial Wire Viewer (SWV) trace function is NOT available for the STM32WL5JC, right?
TIA
2024-04-02 8:50 AM
PB3 = JTDO / TRACE SWO
2024-04-02 12:37 PM
Many thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.