2024-02-14 1:16 AM
Hi Community
Hope you guys are well. I am trying to implement Bluetooth and emulated eeprom working. i have followed the ble_heartrate_eeprom_emul example and i got blue tooth and eeprom emulation working, the problem i am having is when the EEPROM emulation is implement my function in custom_stm.c does not work properly, for example when i used any of the GPIO, the controller goes into hard fault, and current went from 0.013A to 0.150A , but as soon as i remove the eeprom emulation code , everything works perfectly. so basically i cant get my things working when there is eeprom emulation , i have tried to release the semaphore 7 in my function but still the same.
there is one more thing, in app_entry.c we have default code , check file attached,
but the ble heart rate eeprom emulation tell us to put this code, check file attached,
and if i put that code and generate the code again from cubemx it is removed.
Assistance is appreciated!
Solved! Go to Solution.
2024-04-22 12:21 AM
i created a support ticket for it. and they coudnt fix it either. so now i am using external eeprom to store data. but thanks for help
2024-04-16 1:13 AM
Hello @SikandarLF
I've personally tested on the P-Nucleo-WB55 and everything works fine. I suggest you test it using the last Version of the X-Cube and the STM32CubeIDE. If you still have any issue, Please add more details (screenshots, detailed description,...).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-22 12:19 AM
i have been using the latest version but when the emulated eeprom is implemented, if i try to use any gpio mcu goes into hardfault. but emulated eeprom and ble works fine
2024-04-22 12:21 AM
i created a support ticket for it. and they coudnt fix it either. so now i am using external eeprom to store data. but thanks for help
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.