NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello all,I am currently working on the different combinations of LoRa Wan and found out that I-Cube-LRWAN software expansion(https://www.st.com/en/embedded-software/i-cube-lrwan.html). For the stm32l476rg, I used the sx1262dvk1das and sx1276mb1mas a...
Several Issues causing this fail, as I can see from the console.1. First, I used to STMCubeMX to generated code while doing the pin Configuration by my own. STM32WLE5CCU6 is the target device in my case. I followed the schematics to do the pin config...
In general , when does resolving list used by stack and when is the data in bonding list used during pairing?I see that entries can be added by application to the resolving list, something that can't be done to the bonding list.Is there some chart ex...
I have a CubeWL-based, CubeMX-generated LoRaWAN application (868Mhz region) on Helium (LNS tells me RX1 delay is 1s).OTAA join and confirmed msg downlink reception seemed very unreliable, even with a gateway just in the other room (OTAA ± 5 tries, up...
On the STM32WL55 MCUs, is it possible to have the ADC interrupt go only to the Cortex-M0+(CPU2)? I have a situation where I would like to trigger CPU2 with interrupts from the ADC, but I don't want to trigger the ADC interrupt for CPU1. Is this pos...
I am a the peripheral, and just got a connection event from the client.Would like to know if server side provides a feature to know if I already bonded with client , or bonding will be needed. Is there a command I can give e.g., the ConnectionHandle ...
When a peripheral sends an aci_gap_slave_security_req() what event does it generate on central side?Asking it as central has the option to:Encrypt link . "the master may encrypt the link", which command does that?Pairing proc init "initiate the pairi...
how can i do to activate the ble of stm32l4 cardI use platform io and framework = zephyr
Hi, I am using the P-Nucleo-WB55x board and using the latest CubeProgrammer v2.16.0 and I tried to install stm32wb5x_Safeboot_fw.bin since the release note said we need to install this FW. I have this error.-------------10:41:17 : Download Stack/FUS ...
HI, I am developing my ble audio project with STM32WBA55G-DK1. I need use SAI interface as audio input interface. I have an annoying problem. I configure RCC before init ble stack. I choose use pll1rclk as system clock. But i call the BleStack_In...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.