STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! Custom Template BLE and LPM

I everyone ,I'm working on a STM32WB35I've build a small custom server app with just a simple batt level service it works and advertise perfectly if I don't enable LPM as soon as I enable LPM it don't advertise anymoreit looks as if CPU2 and RF are d...

oga_0-1712761048851.png oga_1-1712761081244.png oga_0-1712829155087.png
oga by Associate III
  • 2521 Views
  • 4 replies
  • 0 kudos

STM32WLE5C8U6 ADC wont start

I've been stuck trying setting up an ADC pin on an STM32WLE5C8U6 MCU for several days. Although I'm new to the ST environment, I have experience setting up ADC pins on other F series chips without any issues. Am I possibly overlooking something? Acco...

Nando by Associate
  • 1461 Views
  • 1 replies
  • 0 kudos

OpenOCD remote session fails due to verification

Hi, for a remote dev environment I need to connect to the on-board stlink remotely.when trying to connect I get this error: I already tried this forum solutionhttps://community.st.com/t5/stm32-mcus-boards-and-hardware/how-to-deal-wirh-could-not-verif...

ltoso1_0-1718661600464.png
ltoso.1 by Associate II
  • 2329 Views
  • 3 replies
  • 0 kudos

Resolved! LoRa duty cycle on LoRaWAN_End_Node

I'm working on stm32wl55 Nucleo-64.I have doubts regarding the mechanism by which the duty cycle control is implemented in the project.I am sending a test LoRa message with a payload of 231 Bytes, using DR5 and SF7 every 10 seconds (whereas a 1% duty...

Feanoer by Associate II
  • 2642 Views
  • 1 replies
  • 0 kudos

Issue setting the BLE TX power level

Hello Guys, We are trying to set maximum power for BLE i.e +6 dbm. After setting the power, we are getting max power of +1.74 dBm only. This was measured at the RF output of the SMA connector in the STM32WB55 Nucleo Board dev kit.  Below is the code ...

WB55 USB Dongle Not Seen by CubePgmr In Windows

HelloI have tried to update the FUS, BLE Stack, and the default client app on the dongle.I have now done this several times, with the Clent App not doing what the UM says.But the issue now is that the USB Dongle in Boot0 mode is not seen by windows (...

GRama.2 by Associate III
  • 2597 Views
  • 7 replies
  • 0 kudos

STM32WL NVIC_SystemReset issue.

Dear ST,We found that when we execute NVIC_SystemReset(); there will be a random CPU hang. In order to eliminate the problem of whether it is developed for our program,I used the lorawan at slave routine, and after compiling it directly,When I execut...

Weili by Associate II
  • 1601 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.