NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am trying to make communication between two Lora E5 mini modules. So, I am using SubGhz Ping pong example. I flashed program in two lora e5 modules. In one module, I am always getting HAL_SUBGHZ_ERROR_TIMEOUT in the function SUBGHZSPI_Transmit. Ple...
I'm working on the STM32WL55 Nucleo-64, starting from the LoRaWAN_End_Node.I performed a hexdump and noticed that the ELF file generated at the end of the compilation process contains a significant recurrence of absolute paths, as shown in the pictur...
Hi, I am using a STM32WB15 board for BLE applications. I understand I need to download the correct FUS before I can ask the board for running any programme. However, I find when using UART to connect the board I cannot running the FUS as well as wire...
In STM32cubemonitor-rf, when i click 'connect' buttion,pop-up massege 'Device under test not responding COM port closed'. How can I use the program. please help me.
Hello,I want to read which stack is updated in my controller. For example stm32wb5x_BLE_Stack_full_extended_fw / stm32wb5x_BLE_Stack_light_fw / stm32wb5x_BLE_Zigbee_RFD_static_fw. So can I read back the stack name using code? Is there any way to read...
Hi all,My application is showing belowDevice(NUCLEO-WL55JC1 EVM) send data to Gateway --> wait 100msec --> enter receive to wait data from gateway. In my test, If data from gateway more then device. The device report CRC Error to application layer.I ...
Hello everyone, I want to measure the current consumption in low power modes on a STM32WB5MMDK discovery board, I would have two questions :)1) I have clock issues when I want to use MSI clock to have a 2MHz SysClk to put my STM32 board in Low run p...
My STM32WL55JC2 is programmed with the example code for Lora End Node given in the SDK v1.3.0.Class_A is enabled by default and working properly i.e. receive window of the MCU opens only after the periodic uplink.When the class is set to Class_C in t...
Setup STM32WL55JC1 embedded on a custom PCB with other peripheralsSTM32CubeIDELora gateway - Multitech MTCDT3AC model with a built-in network server, join server, packet forwarder and gateway.STM32CubeWL f/w version 1.3.0 Application hangs because MB...
Hello everyone, I want to measure the current consumption on a STM32WB5MMDK discovery board. I've found that I had to put an ammetre on the jumper JP1, and I programmed the RGB LED to be working. However, when I put the ammetre and I power my board, ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.