STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Couldn't Find Mac_802_15_4_Sniffer.bin file

Hi Community,I’m trying to use the CubeMonitor-RF sniffing tool to monitor packets between my two NUCLEO-WB55 boards. I have followed all the instructions indicated by UM2288 and the ST Wiki. However, I am confused about the firmware upgrade for the ...

iFoX by Associate II
  • 2218 Views
  • 3 replies
  • 0 kudos

Disabling TCXO in the software

I am using the B-L072Z-LRWAN1 and trying to optimize for low power consumption. So far I have set up the hardware by desolding SB37, SB18, R26, and D2. Now when moving JP9 from pos. 2-3 to pos. 1-2 (i.e. TCXO powered from PA12 instead of VDD_RF_LRA),...

Resolved! How to identify two or more BLE devices

Hi, I have a question.I am developing a BLE HIID device using the STM32WB55 evaluation board.I am not sure how to identify multiple devices with the same firmware loaded.The problem I am currently encountering is as follows ↓↓↓.Prepare two CFG_STATIC...

ELEHM by Associate II
  • 2375 Views
  • 3 replies
  • 1 kudos

Resolved! STM32WB55 - input clock for TIM6?

 I am using STM32WB55 with 32 MHz HSE and am trying to find out which input clock frequency I should use for TIM16. Unfortunately it is not clear in the diagram from the datasheet. Where can I get this information? Greetings,Andreas   

AndreasC_0-1721736526957.png
AndreasC by Associate II
  • 2627 Views
  • 4 replies
  • 2 kudos

BLE Router and Server

I have two STM32WB5MM- DK . Using an example for a diffrent board I have configured one of them as router and other as server. I dont know if they are getting connected.  I need to connect these exclusively and then connect the router to Mobile phone...

Rituraj by Senior
  • 2130 Views
  • 6 replies
  • 0 kudos

Resolved! STM32WBA55G-DK1 not compatible with all mobiles

Hi I recently purchased DK board and connected to the phone to check the dumped code.But, I couldn't listen to any music nor call. I realised only few selected mobiles with BLE Audio can be used to test the board.Any solution to this? @STTwo-32 @KDJE...

Pallavi by Associate III
  • 2363 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.