2024-07-22 4:14 AM
Hi
I recently purchased DK board and connected to the phone to check the dumped code.
But, I couldn't listen to any music nor call.
I realised only few selected mobiles with BLE Audio can be used to test the board.
Any solution to this?
@STTwo-32 @KDJEM.1
Thanks in advance!
Solved! Go to Solution.
2024-07-22 11:12 PM
Hi @Andrew Neil
Thank you. Got it!
I have understood that only few mobiles with BLE feature can be used to test the Audio features as mentioned in
2024-07-22 4:23 AM - edited 2024-07-22 4:24 AM
@STTwo-32 has already answered this question for you:
https://community.st.com/t5/stm32-mcus-wireless/classic-bluetooth-in-stm32wba55/m-p/694969
The ST Chips do BLE only; they do not do "Classic" Bluetooth - so you obviously won't be able to use them with phones which only have classic Bluetooth!
@Pallavi wrote:Any solution to this?
You will need a separate Classic BT module to support Classic BT.
2024-07-22 11:12 PM
Hi @Andrew Neil
Thank you. Got it!
I have understood that only few mobiles with BLE feature can be used to test the Audio features as mentioned in
2024-07-23 1:53 AM
Yes, Auracast (LE Audio) is a very new BLE feature (only released this year?) - so very few phones yet support it.
Please mark the solution.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.