2025-03-19 7:52 AM
1. [Part Number] NUCLEO-WL33CC1
2. [Environment] Windows 11 laptop
3. [Schematics] Using ST Nucleo board.
4. [Details] STM32CubeIDE would not enter debug.
5. [Expected behavior] It should enter debug after a power reset regardless of what low power mode
6. [How to reproduce] Simply program standard ST MRSUBG_WakeupRadio_Tx example
7. [Occurrence] The problem is constant
8. [Sanity checks] Changed cable. Confirmed boards with STM32CubeProgrammer.
I found that when I run the default ST MRSUBG_WakeupRadio_Tx example program, I am no longer able to enter debug mode or reprogram the device using the STM32_Programming tools (both GUI and CLI).
Is this expected behavior? If so, I would appreciate an explanation as to why this happens. My assumption is that regardless of how the device enters low power mode, a power cycle reset should allow the debugger to reconnect.
Is there a workaround for this? I find this issue quite frustrating, to be honest.
Many thanks in advance!
Ola
Solved! Go to Solution.
2025-04-10 11:08 AM
Hello @ola
The MRSUBG_WakeupRadio_Tx example does support Low power mode by default with Debug disabled as you can see on the lines 67 and 70. So, to be able to debug this example or Connecting the Board to CubeProgrammer after uploading the example, you should set the CFG_LPM_SUPPORTED macro to 0 and the CFG_DBG_SUPPORTED macro to 1.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-10 11:08 AM
Hello @ola
The MRSUBG_WakeupRadio_Tx example does support Low power mode by default with Debug disabled as you can see on the lines 67 and 70. So, to be able to debug this example or Connecting the Board to CubeProgrammer after uploading the example, you should set the CFG_LPM_SUPPORTED macro to 0 and the CFG_DBG_SUPPORTED macro to 1.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.