STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WL PCB RF Design

Dear ST community,I am developing a PCB design for wireless communication utilizing STM32WLE5CCU6. I have a very basic grasp of RF knowledge, impedance matching for example. I read thoroughly the documents: AN5457 and AN5407 of designing RF layout. I...

Saturn PCB.png Nucleo_PCB_Mark.png
MJaworski by Associate III
  • 1879 Views
  • 1 replies
  • 0 kudos

Resolved! Finding if the BLE stack is running

Hi,I'm relatively new with ST microcontrollers and I'm struggling a bit to find an answer to a question I have.I have some code that reads data from an external source. I need to read some data on startup, as it dictates the some stages of the boot p...

STM32WB55 Bluetooth RF Problem.

I have made a custom STM32WB55 Board taking evaluation board as reference except antenna. The antenna used is SMD chip antenna. We have generated p2p server program from stmcubemx and loaded on evaluation board. It is advertise/connect/pair is workin...

YSN by Senior
  • 4042 Views
  • 9 replies
  • 0 kudos

STM32Cube_FW_WL3_V1.0.0 sigfox inserts the ID and PAC

Hello, I want to apply sigfox on the stm32wl33kcv6 project.I have some questions that I hope you can answer. 1. I have sigfox ID and PAC, how do I write to flash?I have noticed these codes:NO_INIT_SECTION(const uint8_t wl3sfx_nvm_boarddata[FLASH_PAGE...

KiteLee by Associate II
  • 901 Views
  • 1 replies
  • 0 kudos

Resolved! BlueNRG-LPS TIM to synchronize DMA transfert

Hi,I work with STEVAL-DB012VA, anf WISE-Studio over Linux. Starting from the peripheral exemple, I am trying to output a sequence of bits over GPIOB at a specific rate. To do this I am programming the DMA to transfert data from a buffer in memory to ...

Resolved! Cannot write TIM registers

Hi,Using Wise studio Version: 1.3.1_R Build id: 2023_05 on Linux with the STEVAL-IDB012V1 (BlueRNG-LPS dev. kit). I discovered that my instructions to write values in the timer registers have no effect. I found it by tracing the program while watchin...

Resolved! RSSI drop between full and extended BLE stack

We are experiencing an issue with poor RSSI values on our STM32WB55 based custom board. We are normally running the extended ble stack and with only 3 feet between the windows PC and the STM32WB55 board were at RSSI values around -85.  When I switch ...

Not receiving VS_HCI_C2_Ready

Hello, I'm trying to implement a custom BLE Client on a P-Nucleo-WB55 board. The ST P2p_client example runs fine on the board and I could add some traces and do little modifications in it before trying to start my project from scratch with CubeMX. It...

VBess.1 by Associate III
  • 6519 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.