2022-03-14 3:30 PM
Flash
make -f ../gcc/Makefile flash
Reading TouchGFX/application.config
Linking TouchGFX/build/bin/target.elf
Producing additional output formats...
target.hex - Combined internal+external hex
intflash.elf - Internal flash, elf debug
intflash.hex - Internal flash, hex
extflash.bin - External flash, binary
-------------------------------------------------------------------
STM32CubeProgrammer v2.10.0
-------------------------------------------------------------------
ST-LINK SN : 066CFF393934504157073017
ST-LINK FW : V2J39M27
Board : NUCLEO-G071RB
Voltage : 3.23V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Error: Unable to list supported devices
Error: Cannot identify the device
make[1]: *** [_extflash_] Error 1
c:/TouchGFXProjects/MyApplication_5/gcc/include/flash_sections_int_ext.mk:2: recipe for target '_extflash_' failed
../gcc/Makefile:47: recipe for target 'flash' failed
make: *** [flash] Error 2
Failed
Failed
The difference between X-NUCLEO-GFX01M1 and X-NUCLEO-GFX01M2 is a second SPI channel.
2022-03-14 10:18 PM
Issues with the loader have been reported within the last week. Indications are that this is being looked into.
2022-03-15 6:48 AM
Cross linking so I can find later https://community.st.com/s/question/0D53W00001PXOc3SAH/failed-to-list-external-loader
2022-03-15 8:27 AM
UPDATE:
I made a mistake, I installed STM32CubeProgrammer to D:\STMicroelectronics\STM32Cube\STM32CubeProgrammer BUT the *.mk files are hard coded for C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin or the Program Files (x86) for 32 bit installs. To fix that issue I copied D:\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin to C:\Program Files (x86)\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin so I put x64 code in the x86 directory...
I removed the STM32CubeProgrammer from D: and installed in C: TouchGFX works GRREAT!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.