2026-05-20 2:46 AM - last edited on 2026-05-20 3:05 AM by mƎALLEm
Hi All,
I want to do something very basic, but somehow cannot manage to do it.
What happens if you have a PWM signal on an IO Pin, generated by a timer, and you disable the timer?
What happens to the physical IO Pin ? Is it stuck at the state where it was when you disabled it ?, Does it go Low ? Or High. The Idle state of the Timer is Low, and the On state High.
Thanks,
DJ
Solved! Go to Solution.
2026-05-20 2:49 AM
> and you disable the timer?
Define "disable the timer".
If it's clearing TIMx_CR1.CEN, it stops the counter and the related TIMx_CHx pin remains in that state in which it was at that moment.
But you can for example also clear the respective TIMx_CCER.CCxE bit, and that would set the given pin to Hi-Z.
JW
2026-05-20 2:49 AM
> and you disable the timer?
Define "disable the timer".
If it's clearing TIMx_CR1.CEN, it stops the counter and the related TIMx_CHx pin remains in that state in which it was at that moment.
But you can for example also clear the respective TIMx_CCER.CCxE bit, and that would set the given pin to Hi-Z.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.