2019-01-14 5:43 PM
I am wondering if there are any examples or plans to add functionality to the external buttons in TouchGFX Desiger.
In the beginning of last week I succeeded in touch control by applying my GUI to the 746dico board.
And now I am connecting the external interrupter and checking the operation.
When I change the GUI through the TouchGFX designer, the external interrupt code disappears.
So I wonder if there are other methods or examples.
I would like to thank you for using a good program. Thanks to that, I have a new and excellent way to do what I do.
2019-01-14 8:02 PM
I found some video from YouTube(TouchGFX, STMicroelectronics channel).
So I'm studying now.
2019-01-24 7:12 AM
Hi,
Where are you adding your interrupt code? It shouldn't get overridden (only the generated/gui_generated folder). The designer does not directly know how to setup your external interrupts for a particular board. Also, i don't think there are any plans to create "direct" mapping to the buttons that are on a particular board. e.g. USER and RESET for STM32F469-DISCO.
Best regards,
Martin
2019-01-24 4:02 PM
Sorry my explanation was not enough.
I had to code interrupts in model.cpp.
So I expressed it as direct.
Now i'm creating separate cpp and hpp and run them in other tasks.
2019-01-28 2:46 PM
And how are things working out for you now?
2019-01-28 4:50 PM
Yes. The project works as well as I want. Thanks!
2019-01-29 3:55 AM
That's good to hear!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.