2021-04-16 2:29 PM
I have a scree with a modal window. Modal window is set to not visible by default. I want the screen to appear first and after some delay the modal window should appear. I created two interactions like this.
Interaction1:
Trigger = Screen Transition begins
Action = Wait for
Duration = 1000ms
Can trigger another interaction = true
Interaction 2:
Trigger = Another interaction is done
Choose interaction = Interaction1
Action = Show Widget
Choose widget to show = modalWindowName
For some reason, modal window never appears. Please suggest what I am missing.
2021-04-17 12:21 AM
Your miss is Screen Transition begins
change this to ending.
But i test your issue and have next question. Modal window is container, i add to it in designer two next objects button and border box, but this two objects isnt showed. Why?
2021-04-17 5:57 PM
Changing the trigger to "end" didn't help. Same behavior.
May be they in background in your case. I have images, button and a line in my modal window and they show up fine.
2021-04-18 12:23 AM
i test it only on simulator and timed showing for me work without inner objects show.
When your dont, you need debug and check where code block.
I use 4.16.1 for test.
2021-12-14 12:21 PM
In your Screens view, maybe your modal widget is being drawn behind something else. Try making it the first widget below your screen name (and hide it using the Toggle Visibility icon).
2021-12-15 12:09 AM
I dont check , but if exist change this to end not begin
Trigger = Screen Transition begins
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.