2021-12-03 6:28 AM
I'm testing TouchGFX on an STM32WB55 Nucleo Board. I configured the board using CubeMX, and designed a very simple screen in TouchFGX 4.18. I'm using an SPI LCD with ARGB222 format, and a partial buffer (just 1 block of 20 lines). Variable 'memory' is correctly allocated when debugging (MDK_ARM).
Returning from allocateBlock(), the program goes into abort() function (called by _ZN8touchgfx3HAL27configurePartialFrameBufferEtttt).
Am I missing something from the configuration?
Solved! Go to Solution.
2021-12-14 10:55 AM
Ok... looking at the source of simulator I found out that the assertion is coming from the fact that "REFRESH_STRATEGY_PARTIAL_FRAMEBUFFER only supports 16bit or 24bit framebuffer". I missed that in reading the documentation...
2021-12-13 5:04 AM
I'm still stuck into this. I changed the board and the development system, but the problem is still there. CubeMX IDE shows that the problem comes from an assertion at the beginning of library function touchgfx::HAL::configurePartialFrameBuffer().
Is there any chance to know what is checked in that assertion?
2021-12-14 10:55 AM
Ok... looking at the source of simulator I found out that the assertion is coming from the fact that "REFRESH_STRATEGY_PARTIAL_FRAMEBUFFER only supports 16bit or 24bit framebuffer". I missed that in reading the documentation...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.