STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Integrate external code in to TouchGFX engine

I am looking to call a function from TouchGFX engine. This function resides in external code. Ideally, the function should be called from TouchGFX before handleTickEvent() from each screen is called. I would like to know both the ways i.e. call the f...

BGuth.1 by Senior
  • 780 Views
  • 1 replies
  • 0 kudos

Resolved! Frame buffer allocation aborts program

I'm testing TouchGFX on an STM32WB55 Nucleo Board. I configured the board using CubeMX, and designed a very simple screen in TouchFGX 4.18. I'm using an SPI LCD with ARGB222 format, and a partial buffer (just 1 block of 20 lines). Variable 'memory' i...

paolog by Senior
  • 1751 Views
  • 2 replies
  • 0 kudos

Resolved! TGFX 4.18: RAM problem with the new video widget

Dear all,I have a problem with the new video widget in combination with the STM32F769NI-DISCO (MIPI DSI display 800x480 px, JPEG HW en-/decoder, 16 MB ext RAM, 64 MB ext QSPI Flash).If I create with the TGFX designer 4.18 a new video example project ...

Doe John by Associate
  • 1374 Views
  • 1 replies
  • 0 kudos

Resolved! Why is TouchGFX Swipe Threshold inconsistent?

I'm using the STM32F469I-DISCO board with TouchGFX. In portrait mode, I set the swipe threshold to 400 because I want the user to swipe almost all the way across the screen to switch pages. When I swipe slowly, it seems to work. However, a fast swipe...

wired by Senior III
  • 2432 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.