2025-06-10 3:35 PM
Hello.
I've been struggling to flash a simple TouchGFX application through the STM32 VS Code extension. I am using the Nucleo-G071RB dev board with the GFX01M2 display board. My project was initially created using the TouchGFX designer, then generated the CMake project in CubeMX. In VS Code, I added the SPI_FLASH section in STM32G071RBTX_FLASH linker file, and the cmake/touchgfx sub directory in the CMakeLists. This allowed me to build the project with no errors. However, whenever I try to flash, I get the following:
I suspect this has something the do with the external flash. I am aware of an external loader file that you have to select in STM32CubeIDE, but I'm not too sure what would be the equivalent in VS Code.
Solved! Go to Solution.
2025-11-05 2:01 AM
I meant launch.json. I came up with one but it doesn;t work with the STM32Cube plugin of VScode. It only works with the cortex-debug plugin:
2025-11-05 3:29 PM
{
// Use IntelliSense to learn about possible attributes.
// Hover to view descriptions of existing attributes.
// For more information, visit: https://go.microsoft.com/fwlink/?linkid=830387
"version": "0.2.0",
"configurations": [
{
"name": "Build & Debug Microcontroller - ST-Link",
"cwd": "${workspaceFolder}",
"type": "cortex-debug",
"executable": "${command:cmake.launchTargetPath}",
// Let CMake extension decide executable: "${command:cmake.launchTargetPath}"
// Or fixed file path: "${workspaceFolder}/path/to/filename.elf"
"request": "launch",
"servertype": "stlink",
"device": "STM32G071RBTx", //MCU used
"interface": "swd",
"serialNumber": "", //Set ST-Link ID if you use multiple at the same time
"runToEntryPoint": "main",
"svdFile": "${config:STM32VSCodeExtension.cubeCLT.path}/STMicroelectronics_CMSIS_SVD/STM32G071.svd",
"v1": false, //Change it depending on ST Link version
"serverpath": "${config:STM32VSCodeExtension.cubeCLT.path}/STLink-gdb-server/bin/ST-LINK_gdbserver",
"stm32cubeprogrammer":"${config:STM32VSCodeExtension.cubeCLT.path}/STM32CubeProgrammer/bin",
"stlinkPath": "${config:STM32VSCodeExtension.cubeCLT.path}/STLink-gdb-server/bin/ST-LINK_gdbserver",
"armToolchainPath": "${config:STM32VSCodeExtension.cubeCLT.path}/GNU-tools-for-STM32/bin",
"gdbPath":"${config:STM32VSCodeExtension.cubeCLT.path}/GNU-tools-for-STM32/bin/arm-none-eabi-gdb",
"serverArgs": [
"-m","0",
],
//"preLaunchTask": "Build + Flash"
/* If you use external loader, add additional arguments */
//"serverArgs": ["--extload", "path/to/ext/loader.stldr"],
},
{
"name": "Attach to Microcontroller - ST-Link",
"cwd": "${workspaceFolder}",
"type": "cortex-debug",
"executable": "${command:cmake.launchTargetPath}",
// Let CMake extension decide executable: "${command:cmake.launchTargetPath}"
// Or fixed file path: "${workspaceFolder}/path/to/filename.elf"
"request": "attach",
"servertype": "stlink",
"device": "STM32G071RBTx", //MCU used
"interface": "swd",
"serialNumber": "", //Set ST-Link ID if you use multiple at the same time
"runToEntryPoint": "main",
"svdFile": "${config:STM32VSCodeExtension.cubeCLT.path}/STMicroelectronics_CMSIS_SVD/STM32G071.svd",
"v1": false, //Change it depending on ST Link version
"serverpath": "${config:STM32VSCodeExtension.cubeCLT.path}/STLink-gdb-server/bin/ST-LINK_gdbserver",
"stm32cubeprogrammer":"${config:STM32VSCodeExtension.cubeCLT.path}/STM32CubeProgrammer/bin",
"stlinkPath": "${config:STM32VSCodeExtension.cubeCLT.path}/STLink-gdb-server/bin/ST-LINK_gdbserver",
"armToolchainPath": "${config:STM32VSCodeExtension.cubeCLT.path}/GNU-tools-for-STM32/bin",
"gdbPath":"${config:STM32VSCodeExtension.cubeCLT.path}/GNU-tools-for-STM32/bin/arm-none-eabi-gdb",
"serverArgs": [
"-m","0",
],
/* If you use external loader, add additional arguments */
//"serverArgs": ["--extload", "path/to/ext/loader.stldr"],
}
]
}I don't think I touched my launch.json. I just used whatever MX generated.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.