2025-11-05
12:17 AM
- last edited on
2025-11-05
4:28 AM
by
Maxime_MARCHETT
Hardware: STM32H743, SPI2, DMA, TFT: 320×320, RGB565, DMA transfer, MX correctly configured SPI2 interface, CRC, MPU, DMA, touchGFX component...
When creating a new project in Designer, how do I select a template? Or guide me step-by-step to correctly start a HELLO interface.
*This post has been translated from Chinese to comply with the ST Community guidelines.
2025-11-06 12:34 AM
Hello,
Did you already refer to the TouchGFX page here?
2025-11-06 4:32 AM
The basic process for getting started from scratch is outlined here: Board Bring Up Introduction | TouchGFX Documentation.
For an SPI display, this section applies:
3. Display with framebuffer in internal RAM | TouchGFX Documentation
Since the bandwith on single SPI is quite low, you might want to consider using a partial framebuffer, which is explained here:
Lowering Memory Usage with Partial Framebuffer | TouchGFX Documentation
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.