2023-05-18 1:48 PM
I want to implement a bare bones TouchGFX bootloader application that provides text based feedback for status & %programmed.
The idea is for the bootloader to be in FLASH sector0 and for it to be able to program a more complex TouchGFX based application into FLASH sectors1-15 from an image on a SD-card. Trouble is, TouchGFX pulls in lots of stuff not needed for a text based application and so leaves ~20k for the bootloader code after hacking it out manually & turning on full optimisation.
Is there an easy way to build an absolute minimum sized image using TouchGFX with text-only support without hacking generated & library code ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.