2025-10-16 7:30 AM - edited 2025-10-16 7:42 AM
I have been developing code between TouchGFX 4.25.0 Designer and STM32Cube IDE 1.12.1, with the STM32H750DB-DK development kit.
I initially generated the code firstly using TouchGFX, created from the Blank UI using the STM32H750B-DK board setup. I have been successfully been able to create an interface with TouchGFX and then develop the functions within STM32Cube IDE. I have been debugging successfully within the STM32Cube IDE and have created a nice GUI so far.
However, using the generated IOC, that was created using TouchGFX. If I generate the code from the IOC, with minimal changes such as adding TIMER7, it causes the LCD to go to a white screen. After I generate the code from the IOC, I regenerate the code on the TouchGFX.
I require to edit the IOC as I need to add a Timer to control the backlight brightness, but I can't seem to get that far due to generating the IOC causing the white LCD screen problem. I have had to revert my code back at every attempt, to prevent the problem occurring.
Observing debug within the STM32Cube IDE, It seems to get stuck under MX_FMC_InIt, I have compared the MX_FMC_Init, MX_QUADSPI_Init, and MX_LTDC_Init settings, as well as the GPIO pins before IOC generation (where I don't get a white LCD screen), and they are no difference. I have attached a screenshot where it is getting stuck. Do you have any suggestions what could be causing this issue?
Thank you for answering in advance!
Solved! Go to Solution.
2025-10-22 12:54 PM
Hello @AEng7 ,
Could you try using TouchGFX Designer 4.26.0 to check if the issue persists? The TBS version of the STM32H750DB-DK is 3.0.22.
Another suggestion is to verify the priorities in the NVIC configuration table and reduce the TIM7 priority (note: a higher number indicates a lower priority).
2025-10-22 8:40 AM
I have received no response, so I have tagged a couple of ST employees.
Thank you in advance!
2025-10-22 12:54 PM
Hello @AEng7 ,
Could you try using TouchGFX Designer 4.26.0 to check if the issue persists? The TBS version of the STM32H750DB-DK is 3.0.22.
Another suggestion is to verify the priorities in the NVIC configuration table and reduce the TIM7 priority (note: a higher number indicates a lower priority).
2025-11-17 12:27 AM
Hello @AEng7 ,
Any updates about the issue you have faced?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.