2020-11-05 4:43 AM
Hello,
We have problems with the touch screen performance. Is there a way to make this better?
We are using the TouchGFX Example project with the same poor results "Smart Embedded display 7.0" with the "Swipe Container Example".
Basically if I hold my finger on the Swipe Container, the swipe container continuously wiggles left/right even though I am keeping my finger as still as humanly possible. We observe the same behavior with a Slider widget.
We initialize with these settings in our custom application, which then has slightly better performance than the example.
hal.setTouchSampleRate(2);
hal.setFingerSize(20);
hal.setDragThreshold(5);
It seems I have tried every possible combination to try to improve this. Whatever I do, I still get some wiggle. The Example projects perform far worse than this on this display. Any advice would be appreciated.
Even a reference to what settings you guys have had the most success with on other boards would be helpful. Maybe I can use that experience to improve the performance on my board and hopefully get rid of this wiggling. The wiggling/shaking makes the whole product seem it has poorer quality, even though it has some fantastic features/functionality, which are not affected by this. But its the optical impression on the customer which this is really making bad.
Cheers!
Solved! Go to Solution.
2020-11-05 11:18 PM
Resolved.
Setting setFingerSize() and setDragThreshold() to the same value fixed it for us:
hal.setFingerSize(20);
hal.setDragThreshold(20);
2020-11-05 11:18 PM
Resolved.
Setting setFingerSize() and setDragThreshold() to the same value fixed it for us:
hal.setFingerSize(20);
hal.setDragThreshold(20);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.