2020-11-02 2:49 PM
Hi all,
I am developing a project in touchgfx using STM32F429. As the complexity of the project has grown, I have started to see anomalies in the touchgfx.
Until now I have 15 screens and all the screens work fine separately. When I put them all together they also work fine in the beginning, but as I play around from one to the other, after a while touchgfx simulator freezes and closes.
I believe it is some problem with the memory. Somehow, it gets stuck. The code has no obvious bug because the screens work fine separately. I have increased the heap and stack size, however the problem still remains. I checked also the memory required by the CWR, as I draw some rounded corners, but it is way below what I have assigned.
There is one thing which I do not know how to do. And it is related to the teadDownScreen() method, which has an empty implementation by default. I think that I maybe need to run something there so that I can free as much space as possible when I leave one screen.
There is one more thing. I always declare all the components as static, so that touchgfx should know how much memory it needs.
I get the following error when I debug with visual studio:
Exception thrown at 0x008E17E1 in Application.exe: 0xC0000005: Access violation reading location 0x80808098.
And this exception comes always at the following lines:
virtual void backPorchExited()
{
swapFrameBuffers();
tick();
}
Can someone give me a hint on how to overcome this problem?
Thanks a lot for the support.
Bests,
Gazi
2020-11-05 11:47 AM
.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.