2024-11-05 6:44 PM
Hi all,
I used touchGFX before with a STM32F746-DISCO board and that worked fine to get started but now I'm looking to make a custom board with an STM32H7A3 MCU and I see nothing in the touchGFX designer for this MCU. There is an STM32H7B3 DISCO board but that MCU has crypto stuff. I don't care for that. It's been about 2 years since I played with the STM32F746-DISCO board and toughGFX. I didn't see an easy way (like a wizard) to use a custom board back then. I still don't see it now. So ... what to do to use a custom board with a STM32H7A3 MCU? or even a NUCLEO-H7A3...don't see that board in the list of examples either.
thanks
2024-11-07 7:19 AM
Hello @Rodo ,
When you are to use a custom board, you have to follow our board bring up guide .
We don't have a TBS (TouchGFX Board Setup) for all the board such as the STM32H7A3 but you can use the other TBS as inspiration to create your own!
Regards,
2024-11-25 6:26 AM
Hello @Rodo ,
Have you been able to move forward on your issue?
Regards,
2024-11-25 9:34 AM
That's gonna take time but thanks for asking.
2024-11-26 8:48 AM
No problem!
Come back when you feel like it.
Regards,
2024-12-10 6:14 AM
Hello @Rodo ,
Have you had time to work on this?
No pressure, just checking!
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.