2023-12-26 10:57 AM
Hello,
I have a stm32h747i-disco board. When I create a touchGFX project by using touchGFX designer template, it works perfectly. Its color depth is 24-bit and when I change color depth to 16-bit(RGB565), it fails.
To change color depth to 16-bit, firstly I am changing Framebuffer Pixel Format section to RGB565 like in the below:
Then I am changing the Layer 0 - Pixel Format section to RGB565 like in the below:
Before pressing to cubeMX save button, I am deleting target folder. After that, pressing cubeMX save button. Ref: https://community.st.com/t5/stm32-mcus-touch-gfx-and-gui/8-bpp-color-palette/m-p/221627
Later, I am opening touchGFX project and as you can see it is 16-bit now.
Then I am pressing "generate code" button and finally, i'm downloading new 16-bit project to stm32h747-i disco but it shows me this screen when I try to use 16-bit color depth. It fails.
However, when i use 24-bit color depth, it shows me this screen as expected and works without any problem!!!
How can I use STM32H747I-DISCO development board with 16-bit color depth? What am I missing? What should I do? Thank you for all answers!
2023-12-28 1:25 AM
Yes, I did and I checked but no change. What else I can do? I must solve this problem.
2023-12-28 7:32 AM
Well, I'd try disabling TouchGFX and fill the framebuffer with some simple pattern in RGB565 mode to make sure the display is showing what is expected and the hardware settings are ok.
2023-12-28 3:57 PM
OK. I will try. Thank you for your interest!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.