2017-01-30 9:44 PM
I am trying to make communication between
STM32F411RCT6 and character LCD
NHD-C0220BIZ-FS(RGB)-FBW-3VM using I2C protocol.
STM32 is the master and the LCD is slave device. I am using stm32cubemx and HAL libraries for this.
Following is my code so far:
#define LCD_ADDRESS 0x78
uint8_t commands[10] = {0x00,0x38, 0x39, 0x14,0x78,0x5e,0x6d,0x0c,0x01,0x06 };
uint8_t data[4] = { 0x40, 0x61, 0x62,0x63 }; // characters a,b,c to be displayed starting from RAM address 0xHAL_StatusTypeDef halstatus = 0;
void Init_LCD()
{
halstatus = HAL_I2C_IsDeviceReady(&hi2c1,(uint16_t) (LCD_ADDRESS),2,100);
printf('halstatus1 = %d\r\n',halstatus);halstatus = HAL_I2C_Master_Transmit(&hi2c1, (uint16_t)LCD_ADDRESS, commands, 10, 100);
printf('halstatus2 = %d\r\n',halstatus);}
void Show_LCD()
{
halstatus = HAL_I2C_Master_Transmit(&hi2c1, (uint16_t)LCD_ADDRESS, data, 4, 100);
printf('halstatus3 = %d\r\n',halstatus);}
int main(void)
{HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART1_UART_Init(); MX_I2C1_Init();Init_LCD();
Show_LCD();while (1)
{ } }I am getting output as:
halstatus1 = 0;
halstatus2 = 1;
halstatus3 = 1;
I was expecting characters a,b,c to be displayed on the LCD screen, which is not happening.
The
HAL_I2C_Master_Transmit() function fails with HAL_ERROR, it is sending 10 bytes first time and 4 bytes another time.
When I try to send just 2 command bytes usingHAL_I2C_Master_Transmit() instead of 10 bytes, halstatus2 is zero or HAL_OK, but it does not configure my LCD display.
Following is the C code of character LCD given in the data sheet:
/* Initializes the LCD panel. */
void init_LCD(void) { I2C_Start();I2C_out( 0x78 ); // Slave address of the LCD panel.
I2C_out( 0x00 ); // Control byte: all following bytes are commands. I2C_out( 0x38 ); // 8-bit bus, 2-line display, normal instruction mode. delay( 10 );I2C_out( 0x39 ); // 8-bit bus, 2-line display, extension instruction mode.
delay( 10 );I2C_out( 0x14 ); // Bias set to 1/5.
I2C_out( 0x78 ); // Contrast set. I2C_out( 0x5E ); // Icon display on, booster on, contrast set. I2C_out( 0x6D ); // Follower circuit on, amplifier=1? I2C_out( 0x0C ); // Display on, cursor off. I2C_out( 0x01 ); // Clear display. I2C_out( 0x06 ); // Entry mode set to cursor-moves-right. delay( 10 );I2C_Stop();
}/* Writes a 10-char string to the RAM of the LCD. */
void show( unsigned char *text ) { int n;I2C_Start();
I2C_out( 0x78 ); // Slave address of panel.
I2C_out( 0x40 ); // Control byte: data bytes follow, data is RAM data.for( n = 0; n < 10; n++ ) {
I2C_out( *text ); text++; }I2C_Stop();
}void main(void) {
int i;init_LCD();
show('HelloWorld');
while(1)
{} }Please update me why
HAL_I2C_Master_Transmit() is failing with HAL_ERROR two times.
Am I doing wrong somewhere .. ?
Thanks,
#character-lcd #i2c-stm32f4xx #stm32cubemx #stm32f42018-09-25 5:47 AM
I have the same problem and the address you use is a special address defined by i2c specs.
#define LCD_ADDRESS 0x78
Addresses from 0x78 to 0x7B define a address with 10 bits.
I'd like to know if there is a possibility to avoid the 10 bit address in i2c peripheral.
2018-09-25 6:31 AM
That display is based on ST7036, and the I2C address is 8-bit 0x78; that's 0x3C if seen as 7-bit address. The I2C standard does not recognize the 8-bit addresses.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.