2016-01-08 9:36 AM
Hi there,
I'm trying to use the STM32F4 Discovery kit (STM32F4Discovery + BB + CAM [OV9655]; without LCD) to take a 16-bits QVGA (320x240) shot and simply store it in a byte array. Assuming that all DMA and DCMI structures are properly set (which I believe that are; more on that later), a 153600 (320*240*2[=16bits]) byte array is needed, which clearly exceeds the 128K RAM size. With this in mind, and in order to validate my assumptions, I've run a couple of tests using smaller buffer sizes and byte arrays and successfully got partial ''good'' pictures: 320x120 when using a 76800 array and 320x140 with a 89600. As such, what I am now trying (and failing) to do is to use the FLASH memory to allocate the desired 153600 bytes and store the image data into it - although I am now able to r/w from/to the whole array using simple initialization/attribution (e.g.: frame_buffer[0] = 0x10), I can't get the DMA to write to it. Please find the relevant code below.
#define DCMI_DR_ADDRESS 0x50050028
#define FRAME_BUFFER_SIZE 153600
__attribute__((__section__(
''.user_data''
))) uint8_t frame_buffer[FRAME_BUFFER_SIZE] = {0};
// uint8_t frame_buffer[FRAME_BUFFER_SIZE/2] = {0}; // WORKS AS EXPECTED, ALTHOUGH JUST 1/2 IMAGE STORED
uint8_t DCMI_OV9655Config(
void
)
{
I2C1_Config();
I2C_GenerateSTART(I2C1, ENABLE);
while
(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT));
I2C_GenerateSTOP(I2C1, ENABLE);
if
(DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x12, 0x80))
{
return
(0xFF);
}
DCMI_OV9655_QVGASizeSetup();
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS, OV9655_COM7, 0x63);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS, OV9655_COM15, 0x10);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS, OV9655_COM10, 0x08);
DCMI_Config();
return
(0x00);
}
void
I2C1_Config(
void
)
{
GPIO_InitTypeDef GPIO_InitStructure;
I2C_InitTypeDef I2C_InitStruct;
RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource9, GPIO_AF_I2C1);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource8, GPIO_AF_I2C1);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOB, &GPIO_InitStructure);
I2C_DeInit(I2C1);
I2C_Cmd(I2C1, ENABLE);
I2C_InitStruct.I2C_Mode = I2C_Mode_I2C;
I2C_InitStruct.I2C_DutyCycle = I2C_DutyCycle_2;
I2C_InitStruct.I2C_OwnAddress1 = 0xFE;
I2C_InitStruct.I2C_Ack = I2C_Ack_Enable;
I2C_InitStruct.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;
I2C_InitStruct.I2C_ClockSpeed = 30000;
I2C_Init(I2C1, &I2C_InitStruct);
}
void
DCMI_Config(
void
)
{
DCMI_InitTypeDef DCMI_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
DMA_InitTypeDef DMA_InitStructure;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOE |
RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOA, ENABLE);
RCC_AHB2PeriphClockCmd(RCC_AHB2Periph_DCMI, ENABLE);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource0, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource1, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource4, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource5, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource6, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_DCMI);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;
GPIO_Init(GPIOC, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1
| GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6;
GPIO_Init(GPIOE, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_6;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
DCMI_InitStructure.DCMI_CaptureMode = DCMI_CaptureMode_Continuous;
DCMI_InitStructure.DCMI_SynchroMode = DCMI_SynchroMode_Hardware;
DCMI_InitStructure.DCMI_PCKPolarity = DCMI_PCKPolarity_Falling;
DCMI_InitStructure.DCMI_VSPolarity = DCMI_VSPolarity_High;
DCMI_InitStructure.DCMI_HSPolarity = DCMI_HSPolarity_High;
DCMI_InitStructure.DCMI_CaptureRate = DCMI_CaptureRate_All_Frame;
DCMI_InitStructure.DCMI_ExtendedDataMode = DCMI_ExtendedDataMode_8b;
DCMI_Init(&DCMI_InitStructure);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);
DMA_DeInit(DMA2_Stream1);
DMA_InitStructure.DMA_Channel = DMA_Channel_1;
DMA_InitStructure.DMA_PeripheralBaseAddr = DCMI_DR_ADDRESS;
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&frame_buffer;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = FRAME_BUFFER_SIZE/4;
// 320*240/WordSize
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream1, &DMA_InitStructure);
}
int
main()
{
DCMI_Control_IO_Init();
if
(DCMI_OV9655Config() == 0x0)
{
DMA_Cmd(DMA2_Stream1, ENABLE);
DCMI_Cmd(ENABLE);
DCMI_CaptureCmd(ENABLE);
DCMI_CaptureCmd(DISABLE);
for
(i = 0; i < FRAME_BUFFER_SIZE; i++)
{
// frame_buffer[i] = i; // WORKS EVEN WHEN USING FLASH MEMORY. ALL 153600 BYTES BECOME SET AND READABLE
printf
(
''0x%02x\r\n''
, frame_buffer[i]);
}
DCMI_CaptureCmd(ENABLE);
return
0;
}
LD script:
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 896K
DATA (rwx) : ORIGIN = 0x080E0000, LENGTH = 128K
// ADDED
RAM (rwx) : ORIGIN = 0x20000000, LENGTH = 128K
CCM (rwx) : ORIGIN = 0x10000000, LENGTH = 64K
}
SECTIONS
{
// ADDED SECTION
.user_data :
{
. = ALIGN(4);
*(.user_data)
. = ALIGN(4);
} >DATA
...
What am I missing here?
Thank you.
Best regards,
Joao Mauricio
#good-luck-with-that #flash #dma #stm32f4 #quem-não-sabe-é-como-quem-não-vê #tortoise-vs-hare #dcmi
2016-01-08 11:08 AM
I can't get the DMA to write to it.
Yeah, kind of think that's going to be a bit bandwidth limiting, and not going to work. Does the DMA fault, or do you get an overrun error?2016-01-08 12:36 PM
2016-01-08 1:26 PM
You need something with enough RAM to hold the image, or the ability to write it somewhere else quicker than it's coming in. Or use a device with a FIFO on it.
The FLASH read is relatively slow, figure 5-6x slower than the internal SRAM. Writing, if the controller even permits this type of interaction, is about 2700x slower, and I doubt if your pixel clock is below 60 KHz.2016-01-11 10:02 AM
Hello clive1,
Thanks for the enlightenment.Best regards,Joao MauricioWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.