STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

FMC on STM32F4xx for Graphics Applications

Posted on January 18, 2016 at 00:37Hellos,I see there is an inbuiltFMC on the STM32F4x9 MCUs which can interface to various memory types including NAND, NOR , SDR SDRAM. My question is: Is it a good idea to use the NOR or a NAND Flash as a FRAME buf...

STM32F4DIS-CAM: DCIM to FLASH Memory using DMA Issue

Posted on January 08, 2016 at 18:36 Hi there, I'm trying to use the STM32F4 Discovery kit (STM32F4Discovery + BB + CAM [OV9655]; without LCD) to take a 16-bits QVGA (320x240) shot and simply store it in a byte array. Assuming that all DMA...

joao2 by Associate II
  • 2065 Views
  • 4 replies
  • 0 kudos

STemWin LCD Rotation on STM32F429 Discovery

Posted on January 03, 2016 at 07:37Hello,I'm trying to rotate the display on an STM32F429 Discovery board by 90 degrees clockwise.  When I tried to place objects such as text, hline, and vline, the coordinates weren't quite what I expected (in fact,...

ralphj by Associate II
  • 1765 Views
  • 2 replies
  • 0 kudos

STM32L152V8 and LCD_CAPA and external decoupling

Posted on December 21, 2015 at 17:37I have an STM32L152V8 running a large LCD using 1/4 bias and 1/4 duty. It works, but needs a little capacitive decoupling on the bias rails. I am using eternal decoupling pins PA0, PA2 and PA12, have enable extern...

crew by Associate
  • 1463 Views
  • 2 replies
  • 0 kudos

STemWin: using GUI_X_Warn() and GUI_X_ErrorOut()

Posted on February 25, 2014 at 16:34I'm using the STemWin522_CM4_OS_GCC library on a STM32F407 board (our own, testing on a 3240g EVAL).   I have a problem using the precompiled library. It should be possible to define the functions GUI_X_Warn() and...

pertti by Associate II
  • 2902 Views
  • 6 replies
  • 0 kudos

Numeric keypad with STM32F429I-Disco guidance

Posted on December 20, 2015 at 00:09I am exploring STM32F429I-DISCO with touchscreen LCD. I am interested in creating a numeric keypad that can take inputs (and store the values). Preferred tools I would like to understand more are SW4STM32 & emWi...

selmesal by Associate II
  • 997 Views
  • 0 replies
  • 0 kudos

stemWin GUI_BMP_DrawEx Hardfaults

Posted on December 15, 2015 at 20:15Hi everyone, I'm trying to display an image from SD card on a display 800x480px. My image have the same size. I can read and write files from the SD card, so that part is no problem. I can also use stemWin to disp...

oe2 by Associate III
  • 1393 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.