2023-12-03 4:40 AM
Has anyone some sample-projects to integrate these 2 hardware?
I'd need the detailed procedure to use the display with this board.
Thanks in advance.
2023-12-03 7:26 AM
Hello @GPioldi and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I suggest you use the examples of the X-CUBE-DISPLAY Expansion Package. Those examples are tested using the NUCLEO-G071RB and NUCLEO-WB55RG. But you can adapt them to the NUCLEO-F401-RE.
Best Regards
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-03 7:28 AM
Sorry but I don't know how to adapt them to NUCLEO-F401-RE... any suggestion / explanation? Thanks, Giuliano.
2023-12-04 9:10 AM - edited 2023-12-04 9:26 AM
Hello @GPioldi
You can start by understanding how this works. Then, you can make it compatible with your NUCLEO-F401-RE. You have to give attention to differences in hardware, peripheral availability, firmware, security, and tools.
You can also use the NUCLEO-G071RB or the NUCLEO-WB55RG with the examples to start if you are not ready to do an example migration.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-04 9:13 AM
Mainly pins and peripherals.
Suggest getting a board that's already supported directly if you're not prepared to do the porting. Create a project for the NUCLEO-G071RB, observe how it's constructed, and how it uses and configures the pins. Adapt to the equivalent on the F401 board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.