2015-06-30 7:02 AM
Hello,
I'm using stemwin 5.26 on STM32F429IIT6 using LCD controller and freertos. my display is 1024 x 600. I started to implement some simple windows, but I see that refresh of the window causes a visible frame corruption. I made and attached a small video to explain clearly the issue.I saw that using only on later (GUI_NUM_LAYERS 1) seems to cancel the issue. I cannot focus if the problem is in the ltdc configuration, dma2d config or STemWin libs.Here code snippets of what I have in the program.main(){ /*** [.....] ****/ /* Initialize GUI */ GUI_Init(); osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 128); defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL); osThreadDef(GUI_Thread, GUIThread, osPriorityLow, 0, 20 * configMINIMAL_STACK_SIZE); osThreadCreate(osThread(GUI_Thread), NULL); /* Start scheduler */ osKernelStart();} /**************************************************************************************/ static void GUIThread(void const * argument) { GUI_SelectLayer(1); GUI_SetColor (GUI_YELLOW); GUI_FillRect(600,300,1024,600); GUI_SetColor (GUI_BLUE); GUI_FillRect(20,10,500,500); k_InitMenu(); while(1) { LED_Toggle(LED1); LED_Toggle(LED2); GUI_Delay(100); } } /**************************************************************************************/void k_InitMenu(void) { WM_SetCallback(WM_HBKWIN, _cbBk); GUI_SelectLayer(1); WM_CreateWindowAsChild(0, 0, 1000, 25, WM_HBKWIN, WM_CF_SHOW | WM_CF_HASTRANS | WM_CF_MEMDEV, _cbStatus, 0);} /******************************************************************************* * @brief Callback routine of desktop window status. * @param pMsg: pointer to data structure of type WM_MESSAGE * @retval None */static void _cbStatus(WM_MESSAGE * pMsg) { int xSize, ySize; static uint8_t TempStr[50]; static WM_HTIMER hTimerTime; static uint8_t tmp; static uint8_t bmp_res2; RTC_TimeTypeDef RTC_Time; RTC_DateTypeDef RTC_DateStructure; uint8_t sec, min, hour, day, month; uint16_t year; WM_HWIN hWin; hWin = pMsg->hWin; switch (pMsg->MsgId) { case WM_CREATE: hTimerTime = WM_CreateTimer(hWin, ID_TIMER_TIME, 1000, 0); break; case WM_DELETE: WM_DeleteTimer(hTimerTime); break; case WM_TIMER: if( WM_GetTimerId(pMsg->Data.v) == ID_TIMER_TIME) { WM_InvalidateWindow(pMsg->hWin); WM_RestartTimer(pMsg->Data.v, 1000); } break; case WM_PAINT: xSize = WM_GetWindowSizeX(hWin); ySize = WM_GetWindowSizeY(hWin); /* Draw background */ GUI_Clear(); GUI_SetColor(0x008d00); GUI_FillRect(0, 0, xSize , ySize - 3); GUI_SetColor(0x808080); GUI_DrawHLine(ySize - 2, 0, xSize ); GUI_SetColor(0x404040); GUI_DrawHLine(ySize - 1, 0, xSize ); /* Draw time & Date */ GUI_SetTextMode(GUI_TM_TRANS); GUI_SetColor(GUI_WHITE); GUI_SetFont(GUI_FONT_13B_ASCII); k_GetTime(&RTC_Time); sec = RTC_Time.Seconds; min = RTC_Time.Minutes; hour = RTC_Time.Hours; k_GetDate(&RTC_DateStructure); sprintf((char *)TempStr, ''%02d:%02d:%02d'', hour , min, sec); GUI_DispStringAt((char *)TempStr, xSize - 70, 4); year = RTC_DateStructure.Year + 2014; month = RTC_DateStructure.Month; day = RTC_DateStructure.Date; if((day > 0) && (day <= 31) && (month > 0)&& (month <= 12) && (year >= 1900)) {sprintf((char *)TempStr, ''%02d, %s, %04d'', day , strMonth[month-1], year);} else {sprintf((char *)TempStr, ''01, January, 2014'');} GUI_DispStringHCenterAt((char *)TempStr, xSize / 2, 4); GUI_DispStringAt( (char *)TempStr, 50, 4); break; default: WM_DefaultProc(pMsg); break; } } #display-stm32f4-lcd2015-07-07 2:15 AM
After few attempts, I found that reducing the speed of LTDC peripheral can cancel the problem.
My 1024x600 display can support higher clock and the LVDS converted the same. I have to decrease to 20 MHz instead of 32 MHz. Is there some limits I have to consider?Best RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.