STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

stm32f429 with TFT working issue

Posted on August 17, 2015 at 07:59Hi.I had worked with sm32f429 interfaced with SSD1963 controller to drive TFT, for now TFT work good. but it seems and checked if I come on one page and than go to another page and than repeat this process again and...

Porting STMCube project example to run on Coocox ide

Posted on July 25, 2015 at 19:39I am new to ARM and I really want to learn about it. I have the STM32F429ZI discovery board and  I have decided to use gcc with Coocox IDE.I tried to port one of the sample project, STemWin_HelloWorld, that accompanie...

luutey by Associate
  • 1184 Views
  • 1 replies
  • 0 kudos

STM32F746Discovery - STemWin

Posted on July 23, 2015 at 23:51I would humbe ask what is behind WM_SetCreateFlags(WM_CF_MEMDEV) ? Trying to write a very easy application based on example ''STemWin_HelloWord'' with a couple of buttons only I can put any widget to main window ( WM_...

STM32F429 HardFault with STemWin-Flexskin

Posted on July 17, 2015 at 08:58Hi, I'm new with the STM32 MCU and I have a problem on my custom board that I can not solve: the system is an STM32F429ZI with SDRAM and a display, like the STM32F4DIscovery. I work with IAR and I made a little test f...

bettif84 by Associate
  • 1312 Views
  • 1 replies
  • 0 kudos

STM32F4 DCMI and OV9655 Partial Image Read

Posted on July 07, 2015 at 16:53Hello,I started using STM32F4DIS-BB and DIS-CAM module with STM32F4Discovery board. Examples found on web displays camera image on LCD through DMA transfer. But in my project, I will not use LCD. 320x240 pixel image c...

STM32F4 and 1024x600 display refresh problem

Posted on June 30, 2015 at 16:02Hello,I'm using stemwin 5.26 on STM32F429IIT6 using LCD controller and freertos. my display is 1024 x 600. I started to implement some simple windows, but I see that refresh of the window causes a visible frame corrup...

nicola2 by Associate II
  • 1584 Views
  • 1 replies
  • 0 kudos

stemwin i2c problem

Posted on July 03, 2015 at 10:05I download the STM32CubeF1 package and compiled the stemwin hello world demo. It is works fine, everything is ok, but I turn on the i2c1 with HAL driver and connect to LM75 temperature sensor. If I put the i2c1 init a...

STemWin problem with GUI_Exec function

Posted on July 01, 2015 at 23:00 Hello, I'm facing with very strange problem using STemWin library. I don't know if this is problem on my side, on STemWin (ST) side or directly from Segger, so I'm asking here first. What's my id...

tm3341 by Associate II
  • 1182 Views
  • 2 replies
  • 0 kudos

STM32L053R8T6 segment LCD

Posted on June 15, 2015 at 16:33Dear Forumers,Can you help me, how to control a 4x18 (com x seg; direck control) costum design LCD?I searched a lot, but i found mostly graphical LCD-s.Maybe an example?Thanks! #segment-lcd #the-stm32l0-series-embe...

arpad by Associate II
  • 2924 Views
  • 5 replies
  • 0 kudos

STM32F429 LTDC and SDRAM

Posted on June 16, 2015 at 14:26Is it possible to use internal RAM as a frame buffer for LTDC?Where exactly in std lib examples are external RAM and LTDC connected? It seems to me that the code is written on SDRAM address but I cannot find any DMA/D...

predrag10 by Associate II
  • 3076 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.