2014-12-11 8:08 AM
Hi:
I am using the STM3221G-EVAL board and trying to use a a different TFT display than the original that came with the board. The original display is an Ampire display that uses a Ilitek controller ILI9320.
The new display I want to use is a Newhaven display that uses Solomon SSD1963.I have downloaded the STemWinLibrary522 from ST website and tried on the EVAL board. This library is supposedly to be configurable to work with different controllers. However, when I ran the STemWimDemo with the Ampire display works fine, but when I switch over the New Haven display I got vertical colored lines. I have changed the LCDConf_stm322xg_eval.c file so the firmware will switch over the SSD1963 controller.Hardware wise, I made a breakout board to re-route the data lines and control lines and everything there seems to be fine.I found out later that the vertical colored lines could be an initialization problem. When I looked at the code it looks like the STemWinDemo uses its own init code for theILI9320 controller.
My question is: even though the STemWin library support SSD1963, do I need to create my own init code for theinitialization of the
SSD2963 controller?Thanks, #stm3221g-eval #stemwin #ssd19632014-12-11 11:34 AM
2014-12-11 2:01 PM
ok, I got it to work (sort of). But the image appeared mirrored and also rotated 90 degrees. What could be the problem?
Thanks,2017-02-24 6:28 PM
https://arm-stm.blogspot.com/2016/12/ssd1963-init-collection.html
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.