2025-07-07 7:28 AM
Hello,
I downloaded a project on the net to write on a 800x480 tft screen with an ssd1963 driver with an STM32F429 ans TouchGFX, I'm starting with the stm32 and I can't get a display on my screen (the screens are created by TouchGFX), I have another code that works and with which I can write on my screen and the ports on the 2 codes are configured in the same way, can someone help me?
Attached files
Best regards
2025-07-07 7:33 AM - edited 2025-07-07 7:50 AM
Start with bus info how is your display connected. Next good is framebuffer place etc.
And into zip pls skip Drivers, Debug and Middleware folders.
In your main code not exist line to init unreset LCD ...
2025-07-08 5:23 AM
Hello,
My initialization code is present in the LCD_SSD1963.c file and it works because it was tested on another code. I manage to generate the code for my screen with TouchGFX (without compilation errors) but nothing is displayed on the screen. Should my screens be in the Frame buffer?
Best regards
2025-07-10 8:07 AM
Hello @PSEBA.1 ,
So you have a project where you can set the color of your display, but when you try to create a project that uses the same hardware and drivers with TouchGFX added, you are not able to control your display?
In the TouchGFX project, are you at least able to set a solid color on the display?
https://support.touchgfx.com/docs/development/board-bring-up/how-to/03-display-internal
If you are not able to control your display, can you check that you get the correct data on your framebuffer (this would mean it is the data transfer that is the problem).
Then look at https://support.touchgfx.com/docs/development/touchgfx-hal-development/touchgfx-al-development-introduction and https://support.touchgfx.com/docs/development/touchgfx-hal-development/scenarios/scenarios-ltdc-parallel-rgb.
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.