2019-12-11 9:26 AM
Hello, I am working on a project where I need to render a computer screen over internet on an LCD controlled by STM32 MCU, like logging to a remote computer from your computer using teamviewer, SVN or remote desktop.
The LCD I will use is 13.3inch with eDP 1.3 (30 pins) interface, I attached its datasheet.
The remote computer runs GP-OS like windows, Linux, Mac or Android. The first important part of the project will use windows PC.
1- Could you suggest me a proper sdk or embedded software that I can run on a proper STM32 MCU (most probably F7) to render the remote computer like what teamviewer does between 2 computers.
2- Should I interface the LCD directly to the MCU through edp interface (is it supported?) or use edp to dsi(which is supported by many st MCUs) converter for example.
Thanks in advance!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.