2025-06-16 7:39 AM
I have a scrollabe list where each item is a scrollable container.
I'm handling the scrollable container with this logic https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/doscroll-doesn-t-scroll-the-full-text/m-p/813190#M43805 (during handleTickEvent I manually change position of the text via code). Each scrollable container has the Horizontal scroll disable with enableHorizontalScroll(false);
Now, I'm facing this issue https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/event-dispatching-bubbling-and-event-interception/m-p/659244#M36957 where when I want to slide the list, I have to click the tiny portion between two items.
Is there a way to bypass the "scrollable container overrides this method to virtually insert itself as the last child in order to intercept the touch events" as I have disabled the scroll so, no need to intercept the scrollable container's events?
2025-06-17 6:24 AM
I asked something similar in the past.
https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/nested-scrollbase/m-p/805868/highlight/true#M43526
I had to overwrite the ScrollableContainer.
If you figure out new ways to improve it.
Please keep me updated.
We could probably drop it in the shared Widget posts.
2025-06-17 6:31 AM
Hi @Marc_LM
Thanks for your answer. Yes, I was trying to find a solution that doesn't involve rewrite the class...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.