2024-07-24 11:28 PM
Hi everyone,
I'm working on a 320*240 SPI LCD and I need to optimize the memory consumption and the refresh speed on it.
At the moment I'm using 4 partial frame buffer of 9.6kB each (with RGB565 16-bit, so 4800 pixels per buffer), but, when I draw an image with dimension 48*45 (2160 pixels) on a already initialized Screen, the touchGFX calls the write on LCD function 3 times:
1 - 48*20 pixels
2 - 48*20 pixels
3 - 48*5 pixels
There is any way or strategy to draw it in one single transaction?
Solved! Go to Solution.
2024-07-26 3:11 AM
Hello @LMenc.1 ,
Unfortunately, this is handled by the TouchGFX framework; therefore, it is not possible to change the strategy, at least from the TouchGFX side.
Best regards,
2024-07-26 3:11 AM
Hello @LMenc.1 ,
Unfortunately, this is handled by the TouchGFX framework; therefore, it is not possible to change the strategy, at least from the TouchGFX side.
Best regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.