2016-01-24 9:21 PM
Hi ,
I have configured LTDC pins as follows./* Enable the LTDC and DMA2D clocks */ __LTDC_CLK_ENABLE(); __DMA2D_CLK_ENABLE(); /* Enable GPIOs clock */ LTDC_GPIO_CLK_EN; /*** LTDC Pins configuration ***/ GPIO_Init_Structure.Mode = GPIO_MODE_AF_PP; GPIO_Init_Structure.Pull = GPIO_NOPULL; GPIO_Init_Structure.Speed = GPIO_SPEED_FAST; GPIO_Init_Structure.Alternate = GPIO_AF14_LTDC; GPIO_Init_Structure.Pin = LCD_DATA_PINS_1; HAL_GPIO_Init(LCD_DATA_PORT_1, &GPIO_Init_Structure); GPIO_Init_Structure.Pin = LCD_DATA_PINS_2; HAL_GPIO_Init(LCD_DATA_PORT_2, &GPIO_Init_Structure); GPIO_Init_Structure.Pin = LCD_DATA_PINS_3; HAL_GPIO_Init(LCD_DATA_PORT_3, &GPIO_Init_Structure); GPIO_Init_Structure.Pin = LCD_DATA_PINS_4; HAL_GPIO_Init(LCD_DATA_PORT_4, &GPIO_Init_Structure); GPIO_Init_Structure.Pin = LCD_DATA_PINS_5; HAL_GPIO_Init(LCD_DATA_PORT_5, &GPIO_Init_Structure); GPIO_Init_Structure.Pin = LCD_HSYNC_PIN; HAL_GPIO_Init(LCD_HSYNC_PORT, &GPIO_Init_Structure); GPIO_Init_Structure.Pin = LCD_VSYNC_PIN; HAL_GPIO_Init(LCD_VSYNC_PORT, &GPIO_Init_Structure); GPIO_Init_Structure.Pin = LCD_MODE_PIN; HAL_GPIO_Init(LCD_MODE_PORT, &GPIO_Init_Structure); GPIO_Init_Structure.Pin = LCD_CLK_PIN; HAL_GPIO_Init(LCD_CLK_PORT, &GPIO_Init_Structure);But I found that in one of the pins, data is not coming properly when I checked in oscilloscope. (LCD_DATA_PINS_4)&sharpdefine LCD_DATA_PORT_4 GPIOB&sharpdefine LCD_DATA_PINS_4 GPIO_PIN_1I tried to configure the same pins are GPIO and was able to change the pin conditions through debugger.Why is this problem happening?Is this because of the way I configured LTDC? Data signal is active in all the other pins . Connections are tested for continuity. #stm32f429-ltdc-2-layer-lcd-tft2016-01-24 11:55 PM
Problem was due to incorrectly configured pin (alternate function).
Now it is fixed.Thanks,AnoopWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.