2023-10-24 9:02 AM
Hello everyone,
I have Custom board that has STM32H7 controller.
I wanted to interface display module G070ACE-LH3 and i have RGB to LVDS DS90C385AMT/NOPB.
As I am a beginner wanted using Stm32 LTDC interface to bring up the display.
Can anyone help me with that?
#LTDC to LVDS
Solved! Go to Solution.
2023-10-25 12:13 AM
I have made some adapter PCBs for the STM32F769I-EVAL board and one of them also had the DS90C385 on it. Attached is the schematic. Check how your display expects the RGB & Sync data in the LVDS stream and connect the LTDC RGB outputs of your SMT32H7 accordingly to the TxIN0..TXIN27.
2023-10-25 12:13 AM
I have made some adapter PCBs for the STM32F769I-EVAL board and one of them also had the DS90C385 on it. Attached is the schematic. Check how your display expects the RGB & Sync data in the LVDS stream and connect the LTDC RGB outputs of your SMT32H7 accordingly to the TxIN0..TXIN27.
2023-10-27 8:43 AM
Thank you very much @t.decker for providing the inputs.
Can you share me Display source code just to test display working?
2023-11-05 11:15 PM
I don't have test code to share. I followed the application notes of Display/LTDC and example projects.
Start simple: Only LTDC without TouchGFX. Define Background color in CubeMX and if all your timing etc is correct, you will see the color on your screen. Then create a Framebuffer and draw some test pattern into it. When you see the pattern on the screen you are ready to start with TouchGFX.
2024-02-13 9:24 PM
sorry for late reply ,
Now display is working ,adjusted LTDC settings.
Now i need to think how to get touchgfx up and running on this
2024-03-18 11:45 PM
Hi, As i'm searching the same way for interfacing lvds display to stm32f769-disc0..is this schematics can be used for f7-disc0 or should be make changes in sch..??
kindly please, help me,,
thanks in advance
regards ,
jr _ mbed_ er
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.