2021-11-08 2:08 AM
Hi,
I'm using TouchGFX dynamic graph and I want to customize the X-Labels according to my data.
For eg. I add 1000 data points and make 10 labels with 100 interval each. So my Labels come as 100,200,300 ...upto 1000. I want to change labels using a wildcard which picks a variable value from the tickevent function. Basically I want to show time in HH:MM:SS Format on X-Axis.
Is There any example for customizing dynamic graph labels??
2021-11-09 3:37 AM
Can Someone help with this?? Using wildcard with Dynamic Graph Labels. I couldn't find any example regarding the same.
2023-07-19 4:57 AM
I am also looking for this, no answers eh? This has to be a fairly common requirement! I'm trying to display RTC time on the x axis label. I have searched but no example of this has been uncovered. In TGFX 4.22 you cannot set a wildcard to the major X axis label so how can it be implemented?
2023-11-22 10:32 PM - edited 2023-11-22 10:33 PM
Also looking for same "How to Display Time on X-Label in Dynamic Graph" which is common for all application. I have working RTC date and time which I am displaying on corner of screen. Also my graph is updating as per RTC second update, Just want to display mm:ss on X axis. I think they forgot to give wildcard option in major X axis label.
I think ST has no answer of this question, Need to change the controller
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.