2025-08-04 1:42 PM - edited 2025-08-04 2:36 PM
I am trying to update a textArea object from a .c file.
I have been able to open the screen by creating a wrapper, the wrapper also handles the data to update.
The screen is called ResultsView.cpp and the textArea is called textAreaTap
to open the screen i created a wrapper: showResultsScreen()
// ResultsScreenWrapper.cpp
#include "ResultsScreenWrapper.h"
#include <gui/common/FrontendApplication.hpp>
#include <gui/results_screen/ResultsView.hpp>
#include <touchgfx/Application.hpp>
#include <gui/results_screen/ResultsPresenter.hpp>
extern "C" void showResultsScreen()
{
static_cast<FrontendApplication*>(touchgfx::Application::getInstance())->gotoResultsScreenNoTransition();
}
extern "C" void update_results_screen(const char* resultText)
{
auto* app = static_cast<FrontendApplication*>(touchgfx::Application::getInstance());
ResultsPresenter* presenter = static_cast<ResultsPresenter*>(app->getCurrentPresenter());
if (presenter)
{
presenter->updateResults(resultText);
}
}and in:
// ResultsScreenWrapper.h
#ifndef RESULTS_SCREEN_WRAPPER_H
#define RESULTS_SCREEN_WRAPPER_H
#ifdef __cplusplus
extern "C" {
#endif
void showResultsScreen();
//void update_results_screen(const char* resultText, int rpm, bool success);
void update_results_screen(const char* resultText);
#ifdef __cplusplus
}
#endif
#endif // RESULTS_SCREEN_WRAPPER_HI modified FrontendApp to include gotoResultsScreenNoTransition
#include <gui/common/FrontendApplication.hpp>
FrontendApplication::FrontendApplication(Model& m, FrontendHeap& heap)
: FrontendApplicationBase(m, heap)
{
}
void FrontendApplication::gotoResultsScreenNoTransition()
{
FrontendApplicationBase::gotoResultsScreenNoTransition();
}
touchgfx::Presenter* FrontendApplication::getCurrentPresenter()
{
return currentPresenter; // 👈 This is protected in base class, now exposed
}Then in my .c file I call:
showResultsScreen();
and the screen opens and it is initialized correctly with the textAreaTap = "4" as setupScreen is called from:
#include <gui/results_screen/ResultsView.hpp>
#include <touchgfx/Unicode.hpp>
#include "string.h"
#include "stdio.h"
ResultsView::ResultsView()
{
}
void ResultsView::setupScreen()
{
ResultsViewBase::setupScreen();
// Explicitly rebind the wildcard
Unicode::strncpy(textAreaTapUpCountBuffer, "4", TEXTAREATAPUPCOUNT_SIZE);
textAreaTapUpCount.setWildcard(textAreaTapUpCountBuffer);
textAreaTapUpCount.invalidate();
}
void ResultsView::tearDownScreen()
{
ResultsViewBase::tearDownScreen();
}
void ResultsView::applyRunResults(const char* resultText)
{
Unicode::strncpy(textAreaTapUpCountBuffer, "3", TEXTAREATAPUPCOUNT_SIZE);
// textAreaTapUpCount.setWildcard(textAreaTapUpCountBuffer);
printf("Buffer address: %p\n", (void*)textAreaTapUpCountBuffer);
printf("Wildcard address: %p\n", (void*)textAreaTapUpCount.getWildcard());
printf("tapUpCountBuffer: %s\n", textAreaTapUpCountBuffer);
textAreaTapUpCount.setWildcard(textAreaTapUpCountBuffer);
textAreaTapUpCount.invalidate();
}So at this point I know the buffers are setup correctly.
I have a presenter: updateResults to pass data to applyRunResults()
#include <gui/results_screen/ResultsView.hpp>
#include <gui/results_screen/ResultsPresenter.hpp>
ResultsPresenter::ResultsPresenter(ResultsView& v)
: view(v)
{
}
void ResultsPresenter::activate()
{
}
void ResultsPresenter::deactivate()
{
}
void ResultsPresenter::updateResults(const char* resultText)
{
view.applyRunResults(resultText);
}
Issue is when I try to call update_results_screen(); from same .c file (also set up in wrapper above) it will not change textAreaTap to a "3"
I am getting the correct data through resultText, but I just tried to a "3" value to test.
I have verified the correct data is in the buffer and that the addresses are correct. I do not know if the screen will just not validate or if it is trying to update the wrong instance of the screen? Maybe I am going about this the wrong way?
Update: I created a button on the screen, The button does nothing, but when I press it the screen updates and updates the textAreaTap with a "3". So, obviously the screen is not updating without the press?
Solved! Go to Solution.
2025-08-04 2:54 PM
I determined the gui was not updating the screen, because creating and pressing a button causes the screen to update.
apparently, it was trying to update out of sync with the handleTickEvent because it is getting called from a C file.
So to sync it up: flag a pending update in the handelTickEvent
bool pendingUpdate = false;
void ResultsView::applyRunResults(const char* resultText)
{
Unicode::strncpy(textAreaTapUpCountBuffer, "3", TEXTAREATAPUPCOUNT_SIZE);
textAreaTapUpCount.setWildcard(textAreaTapUpCountBuffer);
textAreaTapUpCount.invalidate();
pendingUpdate = true; // Delay redraw until tick
}
void ResultsView::handleTickEvent()
{
if (pendingUpdate)
{
textAreaTapUpCount.invalidate(); // Now this works!
pendingUpdate = false;
}
}
2025-08-04 2:54 PM
I determined the gui was not updating the screen, because creating and pressing a button causes the screen to update.
apparently, it was trying to update out of sync with the handleTickEvent because it is getting called from a C file.
So to sync it up: flag a pending update in the handelTickEvent
bool pendingUpdate = false;
void ResultsView::applyRunResults(const char* resultText)
{
Unicode::strncpy(textAreaTapUpCountBuffer, "3", TEXTAREATAPUPCOUNT_SIZE);
textAreaTapUpCount.setWildcard(textAreaTapUpCountBuffer);
textAreaTapUpCount.invalidate();
pendingUpdate = true; // Delay redraw until tick
}
void ResultsView::handleTickEvent()
{
if (pendingUpdate)
{
textAreaTapUpCount.invalidate(); // Now this works!
pendingUpdate = false;
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.