2021-06-30 8:25 AM
So let say I have a group of radio button like this:
touchgfx::RadioButtonGroup<5> radioButtonGroup1;
And whenever use select every radio button inside the group, I want to trigger the same callback handler.
How can I achieve this?
'
Solved! Go to Solution.
2021-06-30 6:51 PM
Ok finally I got it:
//in .hpp
touchgfx::Callback<MainView, const touchgfx::AbstractButton&> cbRadioBtnGroup;
void cbRadioBtnGroupHandler(const touchgfx::AbstractButton& src);
// in .cpp
MainView::MainView() :
cbRadioBtnGroup(this, &MainView::cbRadioBtnGroupHandler) {
radioButtonGroup.setRadioButtonSelectedHandler(cbRadioBtnGroup);
}
MainView::
void MainView::cbRadioBtnGroupHandler(const touchgfx::AbstractButton& src) {
if(&src == &radioButton1) {
// handle for radioButton1 selection
}
else if(&src == &radionButton2) {
// handle for radioButton2 selection
}
....
else {}
}
2021-06-30 8:28 AM
It looks like only individual callbacks from every button are available
2021-06-30 8:35 AM
so far I did this way but it has build error:
in .hpp
Callback<HomeView, const RadioButtonGroup<5>&, const ClickEvent> cbRadioBtn;
void cbRadioBtnHandler(const RadioButtonGroup<6>& src, const ClickEvent ev) {
// handle selected radio button
}in constructor:
HomeView::HomeView():
cbRadioBtn(this, &HomeView::cbRadioBtnHandler) {
}
HomeView::setupScreen() {
radioButtonGroupParamsList.setRadioButtonSelectedHandler(cbRadioBtn);
}But it has compile errror:
Severity Code Description Project File Line Suppression State
Error (active) E0434 a reference of type "touchgfx::GenericCallback<const touchgfx::AbstractButton &, void, void> &" (not const-qualified) cannot be initialized with a value of type "touchgfx::Callback<HomeView, const touchgfx::RadioButtonGroup<(uint16_t)6U> &, const touchgfx::ClickEvent, void>" Application C:\TouchGFXProjects\LagrevSimulation3\gui\src\home_screen\HomeView.cpp 41
Error C2664 'void touchgfx::RadioButtonGroup<6>::setRadioButtonSelectedHandler(touchgfx::GenericCallback<const touchgfx::AbstractButton &,void,void> &)': cannot convert argument 1 from 'touchgfx::Callback<HomeView,const touchgfx::RadioButtonGroup<6> &,const touchgfx::ClickEvent,void>' to 'touchgfx::GenericCallback<const touchgfx::AbstractButton &,void,void> &' Application c:\touchgfxprojects\lagrevsimulation3\gui\src\home_screen\homeview.cpp 41
2021-06-30 8:58 AM
If that is the case, then the code could be really messy, as I have a lot radio buttons and I don't want each of radio button has separate callback.
But I think it is possible to have a general callback for a group of radio button, since I see class RadioButtonGroup has public member function
voidsetRadioButtonSelectedHandler(GenericCallback< const AbstractButton & > & callback)
https://support.touchgfx.com/docs/api/classes/classtouchgfx_1_1_radio_button_group#public-functions
But, it just I dont know how to use it right
2021-06-30 6:51 PM
Ok finally I got it:
//in .hpp
touchgfx::Callback<MainView, const touchgfx::AbstractButton&> cbRadioBtnGroup;
void cbRadioBtnGroupHandler(const touchgfx::AbstractButton& src);
// in .cpp
MainView::MainView() :
cbRadioBtnGroup(this, &MainView::cbRadioBtnGroupHandler) {
radioButtonGroup.setRadioButtonSelectedHandler(cbRadioBtnGroup);
}
MainView::
void MainView::cbRadioBtnGroupHandler(const touchgfx::AbstractButton& src) {
if(&src == &radioButton1) {
// handle for radioButton1 selection
}
else if(&src == &radionButton2) {
// handle for radioButton2 selection
}
....
else {}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.