2026-03-29 7:51 PM
I have this Riverdi 7-inch display which has a STM32H757XIH6 micro controller. And I am trying to use freertos to run a uart task when a button is tapped on the display. I am running into an issue though with the button response. So I created a virtual function and that works when I tap the button. I created another freertos kernal and have a callback function names UART_Task. I am trying to send a message via a queue to start a process when a button is tapped. When the program runs the GUI displays, but when I tap the button it is unresponsive and does not seem to send the message. I messed around with setting different times on the osDelay within the callback to give the GUI and other tasks time to initialize. I also messed around with the priority of the task as well. No luck though.
Here is the Freertos code that is initialized from the main.c. The MX_FREERTOS_Init() is called in the main.c
/* USER CODE BEGIN Header */
/**
******************************************************************************
* File Name : freertos.c
* Description : Code for freertos applications
******************************************************************************
* @attention
*
* Copyright (c) 2023 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "FreeRTOS.h"
#include "task.h"
#include "main.h"
#include "cmsis_os.h"
#include "queue.h"
#include "stdio.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "fdcan.h"
extern FDCAN_TxHeaderTypeDef TxHeader;
uint8_t TxData[] = {0x10, 0x32, 0x54, 0x76, 0x98, 0x00, 0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, 0x88, 0x99, 0x00};
FDCAN_RxHeaderTypeDef RxHeader;
uint8_t RxData[16];
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN Variables */
/* USER CODE END Variables */
/* Definitions for defaultTask */
osThreadId_t defaultTaskHandle;
const osThreadAttr_t defaultTask_attributes = {
.name = "defaultTask",
.stack_size = 512 * 4,
.priority = (osPriority_t) osPriorityNormal,
};
/* Definitions for VideoTask */
osThreadId_t VideoTaskHandle;
const osThreadAttr_t VideoTask_attributes = {
.name = "VideoTask",
.stack_size = 4096 * 4,
.priority = (osPriority_t) osPriorityLow,
};
/* Definitions for TouchGFXTask */
osThreadId_t TouchGFXTaskHandle;
const osThreadAttr_t TouchGFXTask_attributes = {
.name = "TouchGFXTask",
.stack_size = 8192 * 4,
.priority = (osPriority_t) osPriorityLow,
};
/* Private function prototypes -----------------------------------------------*/
/* USER CODE BEGIN FunctionPrototypes */
/* Definitions for TouchGFXTask */
osThreadId_t UARTTaskHandle;
const osThreadAttr_t UARTTask_attributes = {
.name = "UARTTask",
.stack_size = 128 * 4,
.priority = (osPriority_t) osPriorityBelowNormal,
};
/* USER CODE END FunctionPrototypes */
void StartDefaultTask(void *argument);
extern void videoTaskFunc(void *argument);
extern void TouchGFX_Task(void *argument);
void UART_Task(void* argument);
extern void MX_USB_HOST_Init(void);
void MX_FREERTOS_Init(void); /* (MISRA C 2004 rule 8.1) */
/* Hook prototypes */
void vApplicationIdleHook(void);
void vApplicationStackOverflowHook(xTaskHandle xTask, signed char *pcTaskName);
/* USER CODE BEGIN 2 */
void vApplicationIdleHook( void )
{
/* vApplicationIdleHook() will only be called if configUSE_IDLE_HOOK is set
to 1 in FreeRTOSConfig.h. It will be called on each iteration of the idle
task. It is essential that code added to this hook function never attempts
to block in any way (for example, call xQueueReceive() with a block time
specified, or call vTaskDelay()). If the application makes use of the
vTaskDelete() API function (as this demo application does) then it is also
important that vApplicationIdleHook() is permitted to return to its calling
function, because it is the responsibility of the idle task to clean up
memory allocated by the kernel to any task that has since been deleted. */
}
/* USER CODE END 2 */
/* USER CODE BEGIN 4 */
void vApplicationStackOverflowHook(xTaskHandle xTask, signed char *pcTaskName)
{
/* Run time stack overflow checking is performed if
configCHECK_FOR_STACK_OVERFLOW is defined to 1 or 2. This hook function is
called if a stack overflow is detected. */
}
/* USER CODE END 4 */
/**
* @brief FreeRTOS initialization
* @PAram None
* @retval None
*/
void MX_FREERTOS_Init(void) {
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* USER CODE BEGIN RTOS_MUTEX */
/* add mutexes, ... */
/* USER CODE END RTOS_MUTEX */
/* USER CODE BEGIN RTOS_SEMAPHORES */
/* add semaphores, ... */
/* USER CODE END RTOS_SEMAPHORES */
/* USER CODE BEGIN RTOS_TIMERS */
/* start timers, add new ones, ... */
/* USER CODE END RTOS_TIMERS */
/* USER CODE BEGIN RTOS_QUEUES */
/* add queues, ... */
/* USER CODE END RTOS_QUEUES */
/* Create the thread(s) */
/* creation of defaultTask */
defaultTaskHandle = osThreadNew(StartDefaultTask, NULL, &defaultTask_attributes);
/* creation of VideoTask */
VideoTaskHandle = osThreadNew(videoTaskFunc, NULL, &VideoTask_attributes);
/* creation of TouchGFXTask */
TouchGFXTaskHandle = osThreadNew(TouchGFX_Task, NULL, &TouchGFXTask_attributes);
/* USER CODE BEGIN RTOS_THREADS */
UARTTaskHandle = osThreadNew(UART_Task, NULL, &UARTTask_attributes);
/* USER CODE END RTOS_THREADS */
/* USER CODE BEGIN RTOS_EVENTS */
/* add events, ... */
/* USER CODE END RTOS_EVENTS */
}
/* USER CODE BEGIN Header_StartDefaultTask */
/**
* @brief Function implementing the defaultTask thread.
* @PAram argument: Not used
* @retval None
*/
/* USER CODE END Header_StartDefaultTask */
void StartDefaultTask(void *argument)
{
/* init code for USB_HOST */
MX_USB_HOST_Init();
/* USER CODE BEGIN StartDefaultTask */
/* Infinite loop */
//if (HAL_FDCAN_Start(&hfdcan1) != HAL_OK)
{
/* Start Error */
// Error_Handler();
}
/* Infinite loop */
for(;;)
{
osDelay(1000);
}
}
extern QueueHandle_t queueHandle;
extern unsigned char message[8];
void UART_Task(void* argument) {
osDelay(3000);
/* Infinite loop */
for(;;)
{
if(xQueueReceive(queueHandle, message, 0) == pdPASS)
{
printf("Hello\n");
}
}
}
/* if (HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, &TxData[0]) != HAL_OK)
{
Error_Handler();
}
if (HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, &TxData[8]) != HAL_OK)
{
Error_Handler();
}*/
/* USER CODE END StartDefaultTask */
/* Private application code --------------------------------------------------*/
/* USER CODE BEGIN Application */
/* USER CODE END Application */
And here is where I'm trying to send a message in from my button callback.
#include <gui/screen1_screen/Screen1View.hpp>
#include "stdio.h"
#include "FreeRTOS.h"
#include "queue.h"
extern "C" {
QueueHandle_t queueHandle;
unsigned char message[8] = { "Search\n" };
}
Screen1View::Screen1View()
{
}
void Screen1View::setupScreen()
{
Screen1ViewBase::setupScreen();
}
void Screen1View::tearDownScreen()
{
Screen1ViewBase::tearDownScreen();
}
void Screen1View::searchAndConnectBLE() {
printf("Search");
xQueueSend(queueHandle, message, 0);
}
2026-03-29 9:12 PM
It's hard to judge about custom app behavior without getting deep into details. Here you can find qualified help with your project.
2026-03-30 9:14 AM
Well it seems to be some way that I'm not using FreeRTOS correctly. I'd be happy to dive into deeper details about it. I feel like the st forum is a good place to get help being that it is using an st microcontroller. What can I further elaborate on?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.