2021-05-20 9:50 PM
So I am using STM32f769 Disco board, first I use template project from TouchGFX Designer and so far it is good. But then I realize it is using framebuffer located on external SRAM address 0xC0000000. But I want to change the location to internal RAM e.g. defined as array in the code like:
uint16_t framebuffer[widht*height].
How should I do this?
Solved! Go to Solution.
2021-05-21 5:15 AM
Hi,
You can set the framebuffer address within the generated STM32CubeMX project in the "STMicroelectronics.X-Cube-TouchGFX" configuration under the "Software Packs". You can also do this through code in TouchGFXHAL.cpp by setting the start address in the startFrameBufferAddresses function.
void TouchGFXHAL::initialize()
{
TouchGFXGeneratedHAL::initialize();
setFrameBufferStartAddresses((void*)startAddress, (void*)0, (void*)0);
...
}/Romain
2021-05-21 5:15 AM
Hi,
You can set the framebuffer address within the generated STM32CubeMX project in the "STMicroelectronics.X-Cube-TouchGFX" configuration under the "Software Packs". You can also do this through code in TouchGFXHAL.cpp by setting the start address in the startFrameBufferAddresses function.
void TouchGFXHAL::initialize()
{
TouchGFXGeneratedHAL::initialize();
setFrameBufferStartAddresses((void*)startAddress, (void*)0, (void*)0);
...
}/Romain
2021-05-23 11:30 PM
Thank you @Romain DIELEMAN
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.