STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Touchgfx crash / garbage on screen

I am trying to setup touchgfx on a STM32H743II based custom board. When I run the code, it seems thatonly part of the screen is getting updated with some (wrong) fb dataremaining screen is noiseirrespective of my touchgfx screen color, I always see t...

0693W00000APLJJQA5.jpg

Resolved! TGX: Very large external flash file

Hello,I am using Touchgfx v4.16.1 with an STM32F469 Discovery Board. I used Touchgfx Designer to generate two different applications for the Discovery Board. In both cases when I build the applications using the makefile, the external Flash file th...

CPaye.1 by Associate III
  • 1455 Views
  • 2 replies
  • 0 kudos

STM32L4R9ZITx, MIPI-DSI, Display

Hi I have doubt in MIPI_DSII Have only one lane but my Display has 4 lanes I don't know how to connect them bothPlease help me to interface the display with MCUor Else, please suggest to me some OLED display to interface with this MCU(MIPI-DSI)

0693W00000APOhxQAH.png 0693W00000APOjeQAH.png
Sprak.11 by Associate II
  • 1770 Views
  • 3 replies
  • 0 kudos

STM32F429 OV5640 Double buffer DMA issue

Hi, I'm using a STM32F429ZIT6 controller to interface an OV5640 camera module. I'm interfacing the sensor over 8 channel DCMI. I'm trying to capture RGB565 at high resolution. I'm using DMA with the double buffer on the fly address update feature. I ...

ADani by Associate III
  • 1650 Views
  • 1 replies
  • 0 kudos

Resolved! Corrupt images from the OV5640-STM32F4 interface

I am receiving corrupt images from OV5640-STM32F4. This isn't regular, I get proper images of resolution 320x240 to 5MP, but occasionally I keep receiving corrupt images. The corrupt images are found in all resolution. By corrupt image I mean, someti...

ADani by Associate III
  • 4985 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.