2023-03-30 9:08 PM
i have tried by using touchGFX, when i press the "target run" it's showing failed, but when i do "Run simulator", There is no error in it.
2023-03-31 1:10 AM
Hello @SNC.1,
Could you provide more information about the error message ?
Did you start your project with a TouchGFX Board Setup (from TouchGFXDesigner), or from STM32CubeMX ?
Did you ensure that your board is correctly connected and powered ?
/Yoann
2023-04-02 8:52 PM
i started my project with TouchGFXDesigner.
2023-04-24 4:20 AM
Sorry for the delay,
Are you sure the board is correctly connected and powered ?
/Yoann
2023-04-24 4:43 AM
Hello @SNC.1,
Do you have STM32CubeProgrammer Software installed on your computer? Running on target with TouchGFX Designer requires STM32CubeProgrammer software so if you don't have it, you'll need to install it.
/Osman
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.