2019-12-02 5:00 PM
So who was the bright spark who decided that both encode and decode should use the same callback function names? Duh! Means I can't even make them static to isolate them! Doesn't the JPEG hardware know whether its doing an encode or a decode?
Also, the JPEG utilities have compile time (rather than run time) selection of the image format. So much for encoding RGB565 from a camera and decoding ARGB8888 for animations.
Not happy having to play with (yet more) DMA2D format conversions to address the inadequacy of the interface
2019-12-02 5:31 PM
I don't think the architects/coders here are particularly sophisticated. Let alone familiar with complex requirements of streaming audio/video pipelines, or the system level scope.
Can't you readily overload the context structure/handle passed to the callbacks? You can hide a lot of your per-instance information in there. If you really don't like the library code, refactor it.
If I were you I'd find some of the engineers responsible for the software and IP integration to discuss this with. You're kind of outside the envelope for front line support engineers/developers.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.