2024-09-24 9:46 AM
Hi there TouchGFX team!
I'm working on a GUI that monitors several values, like in the screenshot.
What is the best way to create those gray blocks. Should I add a background image will all the circle + gray boxes + text, and then render the values. Or should I create circle + gray boxes + text using widgets?
Also, whats the best way to create those gray boxes?
Thanks a lot in advance
Solved! Go to Solution.
2024-09-27 6:07 AM
Hello @JPabl.1 ,
As @Peter BENSCH said, if the boxes won't move, you can simply integrate them directly on the background image (if you use a background image).
Otherwise, there is 2 ways to create these boxes :
I hope this helps! :smiling_face_with_smiling_eyes:
If this comment or another on answers your question, I invite you to select it as "best answer".
Regards,
2024-09-26 2:06 AM - edited 2024-09-26 2:06 AM
Well, if the grey boxes with rounded sides and the green circle are static objects, you should define them together as a background image and place the changing numerical values in front of them. This also has the advantage over permanent generation with a widget of saving valuable computing time and thus improving the response time of your overall system.
The question of how you should create these grey boxes depends on whether you want to create them as a background image or with the STM32. In the latter case, you can render them quite time-consuming or calculate them more easily with an STM32U5 with NeoChrom Vector Graphics GPU.
Hope that helps?
Regards
/Peter
2024-09-27 6:07 AM
Hello @JPabl.1 ,
As @Peter BENSCH said, if the boxes won't move, you can simply integrate them directly on the background image (if you use a background image).
Otherwise, there is 2 ways to create these boxes :
I hope this helps! :smiling_face_with_smiling_eyes:
If this comment or another on answers your question, I invite you to select it as "best answer".
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.