2022-04-07 4:50 AM
Hi,
I am trying to implement STemWin v5.22 for an F4 MCU. I made sure to provide a path to the static library and included all the other necessary files. However I still get this error:
../Lib\lib_STemWin522_CM4_GCC.a(GUI_Core.o): In function `GUI__Config':
GUI_Core.c:(.text.GUI__Config+0xc): undefined reference to `GUI_X_Config'
collect2.exe: error: ld returned 1 exit statusGUI_X_Config is defined in GUI.h of the STemWin library, to which there is a path provided.
I don't really understand why there is still an unresolved dependency. Are there other files necessary for this STemWin version? I only got the static library from some online repo, not the official ST website. I don't think this version of STemWin is available anymore
Solved! Go to Solution.
2022-04-07 1:30 PM
> GUI_X_Config is defined in GUI.h
Is it *defined* there, or just *declared*? (ie. is there a function body, or just the header)?
I never used STemWin but isn't GUI_X_Config a function you are supposed to provide in your code? Sort of a callback or insert to GUI__Config, so that user can add some needed initialization on his side? Maybe the related documentation talks about this?
JW
2022-04-07 1:30 PM
> GUI_X_Config is defined in GUI.h
Is it *defined* there, or just *declared*? (ie. is there a function body, or just the header)?
I never used STemWin but isn't GUI_X_Config a function you are supposed to provide in your code? Sort of a callback or insert to GUI__Config, so that user can add some needed initialization on his side? Maybe the related documentation talks about this?
JW
2022-04-07 11:06 PM
this was a good tip, the repo I got the library from wasn't complete it seems. I found another STemWin implementation, where GUIConf.c was provided with the full function.
Thank you!
2024-04-23 7:38 AM
Hi, please where did you find the other STemWin implementation. I am having the same issue.
Thanks in advance
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.