2024-04-24 1:17 AM
Hello everybody.
How can I change the behavior of the base class generator in touchgfx designer?
I need to place part of the classes in an external memory chip. To do this, I modify the base class as follows:
For example:
Original generator code
class Navigator : public NavigatorBase
{
public:
Navigator();
virtual ~Navigator() {}
...
I want to place this class in an external flash memory by adding the code:
#ifndef SIMULATOR
#define QUADSPI_EXT_FLASH_MEMORY __attribute__((section("ExtConstDataSection"))) __attribute__((aligned(1)))
#else //SIMULATOR
#define QUADSPI_EXT_FLASH_MEMORY
#endif //SIMULATOR
class Navigator : public NavigatorBase
{
public:
QUADSPI_EXT_FLASH_MEMORY
Navigator();
virtual ~Navigator() {}
...
It works, but when generating the code in the Touchgfx designer, all my extra code is removed.
How can I generate code in the Touchgfx designer and not clear my extra code?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.