2020-11-05 11:36 PM
I use TouchGFX and STM32H7 system. It needs large font files (chinese + many sizes) which will not fit into internal RAM.
I also need to write log data into flash. I would want to use the same flash to store fonts and store the logging data. But TouchGFX fonts require memory-mapped mode, and storing data requires command mode.
Which option is the best?
I would use STM32H7B0 with 2 external flash option (FW+fonts in external mm-flash, data in external cmd-flash), STM32H7B3 with 1 external flash option (FW in internal flash, Fonts+data in external flash with mode switching between mm/cmd).
Solved! Go to Solution.
2020-11-08 9:03 PM
Hello,
I think both solutions are fine. I believe having 2 physical external flash is more expensive than 1 single external flash. However, you will avoid switching between two modes on a single Flash in this case.
Both are doable and if you choose only 1 physical external flash just set it in command mode only when you want to write. As soon as your write is finished, switch back to memory mapped mode.
/Alexandre
2020-11-08 9:03 PM
Hello,
I think both solutions are fine. I believe having 2 physical external flash is more expensive than 1 single external flash. However, you will avoid switching between two modes on a single Flash in this case.
Both are doable and if you choose only 1 physical external flash just set it in command mode only when you want to write. As soon as your write is finished, switch back to memory mapped mode.
/Alexandre
2020-11-08 11:59 PM
Okay, thank you for clarification!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.